Hi Patrick,
The probe connected in my setup is a TDP1500 - it has 200K differential input resistance, is that fine? https://www.tek.com/en/datasheet/differential-probes
sensor min freq 8/3 = 2.67MHz seems a better fit for our device which operates at…
Part Number: DS90UB936-Q1 Hi -
On page 157 of the DS90UB936-Q1 datasheet, it said the following “Ensure CSI trace length is matched within 5 mils for minimal intra-pair and pair-pair skew. Do the pair-pair skew need to be ≤ 5 mils for the DS90UB936…
The Standard Microcircuit Drawing is a vendor-independent datasheet. The SMD is linked from the product web page; it explains the structure of the PIN in section 1.2.
You would order both of them. HVD233HKX/EM is an engineering sample; footnote 2 in section…
Dear Josh,
Thank you for your support.
we tested with AC/DC boost level 0, it had little difference. You can compare with the eye diagram with upper one.
also I am still reviewing the schematic and layout. Could you simulate the impedance match of USB…
Hi Yutaro,
The ESD ratings for this device are as follows:
HBM: 1.5kV
CDM: 1.5kV
MM: 250V
Below is the qualification report for this device.
SN74AHCT573 Qualification Report
Regards,
Sebastian
Hello John,
Thank you for reply.
I understood the range specified in the datasheet. when I connect no external series inductor on N coil the inductance measure with LCR meter is 0.4uH which is very low and sensor capacitance on LDC0851EVM eval kit PCB…
Sayali,
For trouble-shooting purposes, I entered the parameters from Table 4 (from the LDC0851 EVM User's Guide ) in the spreadsheet sensor design tool. That spreadsheet is attached.
For 2 layers, 7 turns/layer, the latest version of the tool (attached…