Part Number: LM385-2 Hello Team,
I reviewed the datasheet but couldn't spot any variances between LM385MX-2.5/NOPB & LM385BMX-2.5/NOPB. Can you clarify the dissimilarities between these components?
Best regards,
Harsh
Part Number: LM385-2 Other Parts Discussed in Thread: TL431 Tool/software: Customer is looking for p2p device and high temp operation one. Could you kindly offer the suggestion. very thanks.
LM385MX-2.5/NOPB
Regards
Brian
Part Number: LM385-2 Hi Team,
Our customer is looking for the tested limit spec of the reverse breakdown voltage of the LM385M3-2.5/NOPB variant of LM385-2.5-N. The datasheet shows the characteristics for its different variants. However, it does not…
Hi Colin,
this is a shunt regulator. To maintain regulation a minimum current of 20µA must be able to flow into the LM385-2.5.
Let's have an example: If the resistor is chosen to be 75R, then a current of (3.3V - 2.5V) / 75R = 10.7mA will flow through…
Other Parts Discussed in Thread: TL431 Not sure is this is the correct forum to post this query in so apologies in advance if not.
I need a 2.5V reference for my PIC 16F886 project to act as a voltage reference for the Analogue/Digital converters built…
Hi Hsu,
Are you looking for a shunt voltage reference at 2.5V or does any voltage reference work?
For a 2.5V TL431 with Ika(min) of 10uA, we do not have a device that meets those specifications but we do have alternatives.
The ATL431 is 2.5V with…
tlc3702 (working).pdf
The photo is the reel we ordered and has the non-linearity issue. Is the attached datasheet (pdf file) the correct datasheet for the reel? If not, please send me the datasheet representing the part on reel. Thank you. Jay
Other Parts Discussed in Thread: LMP91000 , LM4120 , LM385-ADJ Hello I have the following question
Is possible to reduce the current consumption by changing Vref by Linear Regulator ?
http://www.ti.com/general/docs/lit/getliterature.tsp?genericPartNumber…
Part Number: LM385-1 Other Parts Discussed in Thread: LM4041-N , REF1112 Hey Team,
I have a customer that is using the LM385 (I don't know full part number) for their previous generation handheld Digital Multimeter.
Could you provide any recommendations…
Hey Dan,
LM120K-5.0/883 is indeed obsolete. I've attached the PDN.
We don't have an exact P2P replacement so I'd recommend the UA79 series as the closest alternatives.
~ Aaron
PDN 200824.pdf