Part Number: LM393-N Other Parts Discussed in Thread: LM393
I want to make sure that the input impedance of the input pins is high enough that it won't be affected by the voltage divider circuit I have designed here in the attached snapshot.
Part Number: LM393-N Other Parts Discussed in Thread: LM393 Please answer the following two questions.
①. Please tell me the input impedance and variation of the IN + / IN- terminals. ②. If the input voltage of the IN + / IN- pins is the same (when the…
Part Number: LM393-N Other Parts Discussed in Thread: TEST , LM393B I have a really specific question regarding the DSBGA packaging for the LM393-N...
There is a customer considering this package, but they are nervous about the way these DSBGA packages…
Part Number: LM393 Hello Team,
I would like to make sure the LM393 absolute MAX input voltage range.
Our LM393-N data sheet describes as below.
"The input common-mode voltage or either input signal voltage should not be allowed to go negative by more…
Part Number: LM393-N Other Parts Discussed in Thread: LM393 , LMC6772 , TLV1702
Hello, I am using the LM393-N to try to toggle two voltages: Va and Vb. Va should drop high-to-low at V0=1V, and Vb should rise low-to-high at V0=3V. Va changes correctly…
Part Number: LM393-N Other Parts Discussed in Thread: LM393 Hello,
The below application notes recommends to add a series resistance when putting a large capacitance on a comparator output.
http://www.ti.com/lit/an/snoaa35/snoaa35.pdf
Then I would…
Part Number: LM393-N Hello,
I have a question for LM393-N DSBA package(LM393TLX/NOPB).
The below is from Mechanical data in the datasheet.
Is there any mark on the top of the package to indicate BUMP A1 Corner?
Regards,
Oba
Part Number: LM393-N Other Parts Discussed in Thread: LM393 Hi Experts,
We are using a "Low-Power, Low-Offset Voltage, Dual Comparators" whose part number is "LM393M/NOPB"
I am unable to find ibis models for simulation.
Could you please…
Part Number: LM393-N Hi Sirs,
As title, because we have the opportunity to have +/- 500mV voltage level on input pin.
We have use and saw LM393DR
Recommended Operating Conditions is 0 to (V+)-1.5v.
Absolute Maximum Ratings is -0.3 to 36v
Looks it's not…