Hello,
Yes, LM4128 and LM4132 have same footprints but they do not have same input supply range (less than LM4120). Therefore, these products also are not seen appropriate. Thank you.
Best regards.
Hi Armin,
This application is suitable for a voltage reference. There is many applications where a voltage reference is used as a level shifter due to the precision that it offers over a resistor divider. One of our newer precision references is the …
Hi John,
I'd probably recommend something simple like the uA7805. It should really only require a capacitor on its input and output, and should give you a reasonably stable 5V output over temperature and input supply.
As drawn, for a 50mV trip point…
Other Parts Discussed in Thread: LM4120 , LM4128 , LM4132 I'm looking for the part name of LM4120IM-2.5/NOPB.
This part is not on the datasheet or web. I only see M5-xx as SOT-23 package.
Would you tell me what is this part name ? Also please tell me…
Other Parts Discussed in Thread: ADS1241 , REF5025 I am using an ADS1241 ADC to read some thermocouple in a noisy environment. Since the ADS1241 is directly connected to the outside world, I am using a ADUM3154 to isolate the SPI signals from the microcontroller…