Part Number: LM61495-Q1 Tool/software: Hi expert,
Can you help me test below case about our transient response in 2.1MHz sw frequency?
The normal idle current is 0.6A but peak current is 9.7A in 1ms, the voltage tolerance is 3.3 ± 0.15 V.
Thanks…
Part Number: LM61495-Q1 Hello Team
Greetings!
can you please send the unencrypted model of LM61495-Q1
customer is using LTspice they don't have PSpice
Best Regards
Umesh Aghadate
Part Number: LM61495-Q1 Other Parts Discussed in Thread: LM61495 , LM43600 Hello,
Need Unencrypted PSPICE model (.lib) of LM61495-Q1 for Circuit simulation using Ansys tools. As i am performing Radiated emission simulation for our PCB, hence required unencrypted…
Part Number: LM61495-Q1 Other Parts Discussed in Thread: LM61495 Looking through the datasheet, I see a couple references to I_RATED:
(equation 6)
(equation 4)
Is I_RATED referring to the DC max current rating of my selected inductor or of the model…
Part Number: LM61495-Q1 Hello,
I have two questions related to the LM61495-Q1:
- The maximum junction temperature stated as 150oC, but the thermal shutdown tripping threshold is 168oC Nom. can you please elaborate on that ?
- What's the efficiency of the…