Part Number: LM7322 Hi,
I am evaluating the use of this dual channel Op-Amp in an instrumentation amplifier configuration and wanted to understand the relation of op amp parameters between channels on the same package. Specifically, I wanted to see if…
Part Number: LM7322 Other Parts Discussed in Thread: LM258 , TINA-TI Hi,
I'm using the LM7322 in a non inverting op amp configuration as shown below.
I'm getting output values about 350mV higher than I'm expecting. With a PWM with Von = 5V, Voff=…
Part Number: LM7322 Hi TI expert
I am trying to simulate LM7322 in TINA in a buffer configuration supporting capacitive load of 1nF. The datasheet says it can support capacitive loads of large values. But the transient response to a step input signal…
Part Number: LM7322 Hello
I'm trying to pick an Opamp to implement a buffer circuit. I was running simulations to see how the output of the Opamp would change with input. My input will be a square with variable distortion ie the edge time and amplitude…
Part Number: LM7322 Other Parts Discussed in Thread: LM358 ,
I have a differential mode op-amp being used to attenuate an AC signal down to a reasonable level for a ADC. It has a 1.5v offset. Op amp power is 12v, AC is no more than 30V. Using the LM358…
Part Number: LM7322 Other Parts Discussed in Thread: LM7332 , OPA2192 , OPA2202 Hi,
Our Customer has a question about LM7322 & LM7332.
Are these two OPAMPs guaranteed to be no phase reversal with a large C Load?
Customer requirement is that the input…
Part Number: LM7322 Hi
I would like to have the equivalent circuit for LM7322 input/output, showing protection etc.
This is not part of datasheet as was normal in the early days. Where may I find this information.
Breg
Vidar
Part Number: LM7322 Other Parts Discussed in Thread: LM7321 Hi.
We have noticed a voltage (2.6V) on the IN+ when we apply 5V on the IN- and we got confused by this. is this expected behaviour and is it safe to run it like this?
BR // Per
Part Number: LM7322 Other Parts Discussed in Thread: OPA1622 , TLV376 Hi
I am using LM7322QMA/NOPB which is a dual op amp. I have connected both op amps in non inverting configuration and i have used 402 ohm resistors to set a gain of 2.
if i apply for…