Other Parts Discussed in Thread: LM8330 HI~
When use LM8330 EVM,have four question.
Details such as additional file.
LM8330 question _20150521.xlsx
BR
Mars lin
Other Parts Discussed in Thread: TCA8418 , LM8330 , LM8333 , TCA8418E Hi team,
Do we have alternative for ADP5585ACPZ, which is a Keypad Decoder and I/O Expansion?
Regards,
Hailiang
Part Number: TCA8418E Other Parts Discussed in Thread: TCA8418 , LM8330 Hello
TCA8418E and TCA8418 are out of stock,Would you please recommand other TI chip to replace them,Thanks
Rajesh,
Rajesh Kumar72 said:
Do you have any other keypad scan IC to interface membrane matrix switch with adjustable/programmable debounce time?
Take a look at LM8330 and LM8333 and see if they fit your needs.
Rajesh Kumar72 said:
In that case, we would…
Part Number: TCA8418 Other Parts Discussed in Thread: LM8330 , TCA6507 Does TI have a part similar to the TCA8418, TCA6507, or LM8330 that has a SPI-GPIO expander capability?
Thanks!
Hi Max,
Thanks for the suggestion.
But, LM8330 is a 0.4mm pitch BGA part. As informed you earlier, we have a constraint on using BGA part.
Please suggest a Non-BGA part if any. I will parallelly check for some other alternative too.
Regards,
Gireesh
Other Parts Discussed in Thread: LM8330 Dear Sirs
Does TI provide I2C product portfolio with PWM input?
I find some product like LM8330 but LM8330 only suport PWM output.
BRS
Nat
Other Parts Discussed in Thread: LM8330 , TCA6408 Dear Sirs
Does TI provide I2C product portfolio with PWM input?
The application is LIGHT-TO-FREQUENCY (LIGHT SENSOR). The output of LIGHT SENSOR is PWM output. And My MCU only support I2C interface. Thanks …
Emrys,
I have a similar question.
I got three PWMs coming out of LM8330, and I need to boost it up to be 12V PWM.
LM8330 is power with a 1.8Vdc, so I assume that the PWMs is at 1.8Vdc.
Is there some part from TI that I can use for that...?
I'm looking…