Noel-san, Timothy-san,
Thank you for reply.
> I wanted to see if this issue was still present? Yes,,, I'd like to clarify the reason.
> do you have the understanding that TOF is aligned Yes, I think TOF is aligned, because LMH1983 register ALIGN STATUS…
Part Number: LMH1983 Hi team,
I got a question from customer.
I am using the LMH1983 in a product design. In this application we are only using the HIN reference input. VIN and FIN are both tied low. The HIN reference is a 10MHz clock. We are setting…
Part Number: LMH1983 Hello Expert, My customer is considering LMH1983. We think 0x1C(Loss of Lock Threshold) and 0x2D(Lock Step Size) is the setting of judging whether PLL is locked. In their evaluation, then they used 0x1C and 0x2D register as default setting…
Part Number: LMH1983 Hello Support team,
Can LMH1983 support 12G-SDI clock requirements?
Is it necessary to put any jitter cleaner to 12G SDI driver and equalizer?
If it is true, please let me know the proper jitter cleaners.
Best Regards,
Hirokazu Ta…
Part Number: LMH1983 Hi, Good day. Our customer has a similar question about the dimension and distance between the mounting holes of the SD1983EVK. Thus, I have referred them to the original post. However, they say that the dimensions indicated in the…
Part Number: LMH1983 Hi team,
Our customer is requesting the 4 holes size and position information of LMH1983 Evaluation Kit ( https://www.ti.com/tool/SD1983EVK) . Please help in providing the information. Thank you. Regards, Carlo
Part Number: LMH1983 Hi all Would you mind if we ask LMH1983? ■Question1■
During one or two years, did LMH1983 have any design change?
If you have design change like as - process change, test programming change or assembly line, could you share us these…
Part Number: LMH1983 Hi Team,
My customer has some technical questions regarding the LMH1983 sync stripper. They are currently experiencing occasional locking issues with certain parts, in the presence of active video. Replacing the part with another one…
Part Number: LMH1983 Hello Support team,
After the process of Power on -> clock input to Vsync and Hsync -> I2C confutation How long time is it required to make the output clocks (148.35MHz NT, 148.5MHz PAL) follow the input signals? How long time…
Part Number: LMH1983 Hi team,
Does the I2C of LMH1983 support the following frequency?
I2C clock frequency
- Fast-Mode : Max 400kHz
- Fast-Mode Plus : Max 1,000kHz
Regards,
Yamaguchi