Part Number: ADC12020 Other Parts Discussed in Thread: LMH6550
Tool/software:
In the ADC12020 DataSheet, figure 40 shows an example circuit of the chip, in which a differential driver circuit is used. The driver circuit uses LMH6550 with a Vcm end, which…
Part Number: LMH6550 Hi Team,
My customer s looking for the complete thermal data for the device LMH6550MA/NOPB. I've checked the datasheet and it seems the information listed is limited. Can you share the complete thermal resistance data of this device…
Part Number: LMH6550 Hi,
I am in need of the junction to case resistance for LMH6550. I see that the data sheet only lists the junction to ambient resistance.
Thanks!
Part Number: LMH6550 Hi,
I currently have the following circuit set-up (see pic). The amplifier is overheating during operation (with no signal at output) and I've checked all pins (non-floating except pin 7, which based on the datasheet can be left floating…
Other Parts Discussed in Thread: LMH6550 Hi
I'm simulating a circuit in TINA of the LMH6550 in two stages. I am looking for a transient analysis and keep getting the error message component and/or parameter not selected. I do get no error with AC analysis…
Hi,
When I want to open LMH6550 footprint with Ultra Librarian I keep getting this error: This footprint does not exist in the current library, or the component does not have footprint assigned. Footprint Name: M08A_L”. I wonder where I can get the proper…
Other Parts Discussed in Thread: LMH6550 , TINA-TI , LMH730154 Hi Folks,
I'm designing a board that takes in a single ended signal and going through a relay (SPDT) to choose between going to the input of a mux directly and to an ADC/DAC or converting to…
Oh and I found an old FDA parametric table for the TI/NSM parts - that middle section might be of interest to you - the upper section of higher supply parts shows the LMH6550 row, with the LMH6551 a related but slower part, The THS4541 is about twice…
Hi Shridhar,
This request for information was somehow missed till now. Is this issue still open?
With a voltage feedback device like LMH6550, the rule of thumb says that the GBWP stays constant. So, if Av=+6 bandwidth is around 70MHz, you'd expect Av…
Hi Simi,
I'm looking at the datasheet of the LMH6550. I see it can be used to approximate LMP8350 in HP mode. however, my application is using MP mode.
Also, the input offset voltage (differential) of the LMH6550 is typically 1mV. About the same…