Part Number: LMH6654 Other Parts Discussed in Thread: LMH6628QML-SP , LM6172QML-SP , LM7171QML-SP Need an equivalent opamp for space as the LT6200 from ADI or LMH6654 which should be pin to pin compatible.
Part Number: LMH6654 Other Parts Discussed in Thread: LMH6624 , OPA818 Hello friends,
We are looking for a replacement op-amp for LMH6654, because its operating temperature is too low.
The working frequency is 13.6MHz.
The following conditions…
Part Number: LMH6654 Tool/software: Dear Texas Instruments Community,
I am a master's student at the University of Padua currently collaborating with the LEGEND-200 experiment as part of my thesis project. I am simulating the response of the experiment…
Part Number: LMH6654 I'm working on a wide bandwidth signal amplifier. I want to use the LMH6654MF/NOPB as the final output stage. The last amplifier I used had an issue where it worked normally with a 50 ohm DC load, but when the output was AC coupled…
Part Number: LMH6654 Hi,
When the LMH6654 is off (no voltage on V, V-), how much leakage/ off current can be observed on the input pins (IN+/-) when a 1V -3.2V is applied? - the part is configured as unity gain buffer.
Are there protection diodes…
Part Number: LMH6654 Other Parts Discussed in Thread: LMH6723 Hello,
I'm currently using the LMH6654 in a prototype Load Transient Circuit for testing high power regulators. The amplifier drives a discrete AB output stage which then switches some load…
Just another question concerning the LMH6654 , I see that the voltage allowed on the input pins is (V+) + 0.5 while the Vin differential is +- 1.2 . does this effectively mean that if I place a 0.5 DC voltage on my non-inverting input anything above 1…
Part Number: LMH6628QML-SP Other Parts Discussed in Thread: LMH6628 , , LMH5401 , LMH6654 , LMH6702 , LMH6639
Tool/software:
Hi TI-Team,
we have a radiation (SET) issue with LMH6628 in an analysis. Therefore, we are searching for a solution. We…