Part Number: LMK00334-Q1 Tool/software: Hi, Can you tell me what the V differential peak to peak min and max output amplitudes is for the LMK00334-Q1? I have a unique application and need to know the worse case V differential peak to peak min and max output…
Part Number: LMK00334 Hello team,
My customer does not plan to use CLKin1, OSCin, OSCout pins.
What should they do to those unused pins? Should they connect them to GND or leave them floating?
Best Regards, Kei Kuwahara
Part Number: LMK00334-Q1 Other Parts Discussed in Thread: LMK00334 , LMK00304 LMK00334 clock buffer datasheet implied that CLKIN can support HCSL clock, however Vild_min = GND.
Most HCSL clock outputs shows Vol_min = -0.15V (including the LMK00334 - see…
Part Number: LMK00334 Dear TI Team:
We have LMK00334RTVR design in our project,
Now we have trace impedance 85ohmm for CLKin0/n,
trace impedance 100ohm for CLKin1/n
trace impedance 100ohm for CLKoutA0/n
trace impedance 85ohm for CLKoutA1/n
1. Is it ok…
Part Number: LMK00334-Q1 Other Parts Discussed in Thread: LMK00334 Hello,
Can you please confirm:
1) No concern needed to have two or three cascaded LMK00334 for the PCIe Gen2 clock distribution;
2) between two cascaded LMK00334, the output to input termination…
Part Number: LMK00334 Hello team,
Can this device input 3.3V single-end clock?
On datasheet, the single end input voltage swing is 2Vpp (Max).
But this device is capable of LVCMOS input, so I am confused.
Best Regards, Kei Kuwahara
Part Number: LMK00334 Hello,
For the LMK00334 IC, I want to use bank A output only. So that when a bank B & C is not in use, can the VCCOB & VCCOC pin be left unconnected, or is there a recommended procedure?
Part Number: LMK00304 Other Parts Discussed in Thread: LMK00338 , LMK00334 , LMKDB1104 Hello,
I am working on a PCIE clock distribution design for our new network switch board. I have the following requirements: - common clock design - support a mix of Gen…
David,
I see now that you are trying to implement a DC-Coupled LVCMOS input from the datasheet .
1. The CLKIN will be set according to the Single-Ended input you are describing, with CLKin0 toggling and CLKin0* set at ((Vo, pp)/2) *.5. But the output,…
Part Number: LMK00334-Q1 Hi Team,
My customer is looking for 2~3ch Clock buffer with TCXO input ( 52Mhz, Clipped Sinewave) for their system.
it is Automotive application.
Please check the LMK00334-Q1 with this spec and recommend other device if it is not…