Part Number: LMK00804B-Q1 Other Parts Discussed in Thread: LMK1C1104A , LMK1C1104
Hi Experts,
We have customer, would like to confirm if the 1.8V clock signal is okay to input at CLK_P single-ended of LMK00804B-Q1 as shown:
Thank you.
Regards…
Part Number: LMK00804B-Q1 Tool/software: Hi,
We are considering a circuit that uses the LMK00804B-Q1 as a receiver to input an LVDS signal. In the circuit we are considering, we assume that the input signal to the LMK00804B-Q1 will be a differential…
Part Number: LMK00804B-Q1 Tool/software: Hello team,
Can I connect the CLK_SEL pin to the CMOS output via 1kΩ resistor like figure below?
On the datasheet, it says "Clock select input. Typically connected to VDD with an external 1-kΩ pullup. When…
Part Number: LMK00804B-Q1 Tool/software: HI BU team
My customer is developing the multi-line flash Lidar application. They need a pwm signals to fanout to the coming MOS drivers.
The PWM waveform is shown in below screenshot.
The pwm signals is…
Part Number: LMK00804B-Q1 Other Parts Discussed in Thread: LMK00804B Hello,
1. Customer is requesting if it's possible to use a 1.8V Clock input with this device.
2. They would also like to "Daisy Chain" first LMK00804B output to second LMK00804B…
Part Number: LMK00804B-Q1 hello,
my circuit design as below for your reference; now the VDDO is 1v8, the Q2 connect with FPGA I/O via two resistors dividing voltage (because the FPGA I/O input voltage scope is 1V-1.8V) ,I want to keep the FPGA input…
Part Number: LMK00804B-Q1 Other Parts Discussed in Thread: SN74LVC1G74 , LMR33620-Q1 , , TPS745-Q1 Hi, in my design I use several components from texas, like: LMK00804B-Q1, LMR33620-Q1, TPS745-Q1, LSF0108QPWRQ1, SN74LVC1G74, UCC5350MC-Q1 among others…
Hello Arshad,
Arshad Mughal said: 1. Can I directly connect the TCXO (LVCMOS) output with an output impedance of 200 ohm to LMK00804B LVCMOS_CLK input (pin 8) as shown below? Considering driver and transmission line impedance will be different?
That…
Part Number: LMK00804B-Q1 Other Parts Discussed in Thread: LMK00804B Hi.
Can we get a Phase noise plot of LMK00804B-Q1 for 100MHz or 125MHz?
Just as it's available in datasheet of LMK00804B for 125MHz.
Thanks,
Sutej.