Part Number: LMK04616 Other Parts Discussed in Thread: LMK05318B , LMK5C33216 , LMK5B12204 , LMK05028 , CDCDB2000 Hi team,
I am looking for replacement solution for 8A34001E-000AJG8 and 9ZXL0451EKILFT. Do you have recommendation solution for it?
https://www…
Part Number: LMK04616 I am Koki Tsushima who is NCG's FAA.
When I was sorting the jetter cleaners on TI.com, this device is Single-loop PLL.
https://www.ti.com/clocks-timing/jitter-cleaners-synchronizers/products.html#p404=Cascaded%20PLLs;Clock%20network…
Part Number: LMK04616 Dear team
We plan to use the LMK04616 in PLL2 only mode, with OSCin, for both ZDM and pure buffer mode. And we have some confuse as below:
1. In ZDM mode, the feedback channel is CH7/8 or CH 6/9?
2. In ZDM mode, and also need to…
Part Number: LMK04616 Hi,
In SNAU222 there is multi-device synchronization circuit using two LMK04616. One device providing DEVCLK and the other SYSREF. What is the best to configure and program these devices?
At the moment, I have one device configured…
Part Number: LMK04616 Other Parts Discussed in Thread: LMX2594 , LMK61E2EVM Hello,
I am incorporating a clock distribution design to effect the synchronization of multiple ADC tiles. Initially, the design will utilize the LMK04616EVM eval board, which…
Part Number: LMK04616 Other Parts Discussed in Thread: USB2ANY Hello,
I am not able to configure the LMK04616 SPI interface in 3-wire mode. Could you give the access sequence to enable it.
NB. The device works OK if I use the 4-wire interface
Part Number: DAC38RF83
Hi
Just to be sure.
How many SYSREF triggers the DAC38RF83 received, if the SYSREF input goes from logic '0' to logic '1' and stay at '1'?
Thanks
Moti Cohen
DSIT
Part Number: LMK04616 Hi
I want to connect the CLKOUT to OSCIN.
instead of LVDS driver it is LKM04616 4mA HSDS.
Can I use the attached termination and coupling?
Thank
shlomi
Part Number: LMK04616 Other Parts Discussed in Thread: CDCLVP1204 Hello, I'm looking for how to properly connect in AC-coupled a CLKOUT output of the LMK04616 with an input of the CDCLVP1204. Both components do not seem to be electrically compatible…
Part Number: LMK04616 Hi to TI team
I have question about propagation delay at LMK04616ZCRT clock distrabuter.
According TI help desk, the propagation delay between OSCin to CLKout at zero-delay is ~8nS, but the clock phase between those pins is ~0nS. …