Part Number: LMK04616 Hi
I want to connect the CLKOUT7 to the next LMK04616 SYNC.
Do you have a suggestion about the buffer\translator I can use?
Thank,
Shlomi
Part Number: LMK04616 Other Parts Discussed in Thread: LMK04832 Hello,
We have found a major source of phase variation in our system, which is that the "REF-to-out" phase of the PLL that we use to lock to the 250 MHz distributed from the LMK04616 to produce…
Part Number: LMK04616 Other Parts Discussed in Thread: DAC38RF83 Hi
How can I connect an HSDS 4mA or 8mA (out clk from LMK04616) to DAC38RF83 that can receive ecl\lvpecl ?
Can I connect them with AC couple only or I need resistor termination?
At the…
Part Number: LMK04616 We’re using an LMK04616 in a single stage configuration (bypassing the first stage). We found that we have to add a 100ms delay during the initialization steps for the device to function correctly and we’d like to know if this…
Part Number: LMK04616 If we use 3.3V to power the outputs of the LMK4610/16, does the 6-mA HSDS output range still far within the specified 0.72V to 1.06V or is that only if 1.8V is supplied?
Part Number: LMK04616 Hi all. I have some question about LMK04616, so please help me. 1. What are C4, R4 at PLL2? For 4rd Filter? I could not find the explanation in datasheet. 2. Register 0xAF and 0xB0, I want to know enable status. Which is bit that PLL2_RDIV_CLKEN…
Part Number: LMK04832 Other Parts Discussed in Thread: LMK04616 , LMK04610 hello
The frequency range of VCO0 and VCO1, as shown in the datasheet, with output divider values up to 1023 for clk output, Seem that I cannot obtain frequencies lower than 3M…
Part Number: LMK04616 Hi all. I use Zero-delay Mode at CLKout7/8. Where do CLKout7 and CLKout8 connect loop back? I think it connects to PLL1 PFD. Best Regards, Sho
Part Number: LMK04616 Other Parts Discussed in Thread: LMK04828 Hi all,
Using a LMK04616 I need to issue a SYSREF using a SPI trigger, but very frequently the SYSREF signal is not generated after the trigger.
The following is the sequence performed, after…