Hello Derek,
That was very helpful, thanks for the insight.
When you said "the learning curve on these devices can be steep, especially for the supporting software," was that comment specific to the LMK04616 and LMK04610, meaning they are more of a handful…
Hi BR,
Bit 0 in 0xAF is PLL2_RDIV_CLKEN, which enables the clock to the R divider mux. I'm unsure why this isn't disclosed, as it is required for using the R divider. Likewise, bit 0 in 0xB0 is PLL2_NDIV_CLKEN, which enables the clock to the N divider…
Part Number: DAC38RF83 Other Parts Discussed in Thread: LMK04616 , , LMK04828 Hi
I want to connect the LMK04616 to SYSREF+/-, DACCLK+/- inputs.
The LMK04616 outputs are 8mA HDSD, 4mA HDSD and 16mA HCSL.
Which of the option I need to use and what kind coupling…
Part Number: LMX2594 Other Parts Discussed in Thread: LMK04616 Hi
Can I transmit a single end RFout? (RFoutAP)
What am I need to do with the left RFOUT? (RFoutAM, RFoutBM and RFoutBP)
My RFOUT frequency 5760MHz
OSC in 240MHz (from LMK04616 HSDS 4/8 mA)
…
Part Number: LMK04616EVM Other Parts Discussed in Thread: LMK04616 , Hello,
I'm currently working on a design using the clock generator LMK04616, It would be of a great help to get the BOM of the Evaluation Module LMK04616EVM. Could you provide it to me…
Part Number: LMK04616 Other Parts Discussed in Thread: DAC38RF83 , , LMX2594 Hi,
I have attached a block diagram of what I intented to design .
Can someone review it?
I need to connect 8 DAC38RF83 with JESD204B.
The first LMK04616 is PLL2 only and the FPGA…
Part Number: LMK04610 Other Parts Discussed in Thread: LMK04616 , USB2ANY Dear TI
I am using TICS Pro software to configure the clock of LMK04610. I use OSCIN as the input 10M and output 10M, but I will not configure the TICS Pro software. so,I hope you…
Part Number: LMK04828 Other Parts Discussed in Thread: LMK04832 , LMK04616 , LMK00804BEVM , LMK1C1104 , LMK00804B
In a recent post, I was seeking assistance in deciding between a few different devices (LMK04832, LMK04828, and LMK04616) to serve as a master…
Part Number: LMK04610 Other Parts Discussed in Thread: SN74AXC4T245 , LMK04616 , LMK1C1104 , LMK00105 , LMK00101 Hi,
I have 3 question regarding the LMK04610:
Can I use the SPI and all other controls as 3.3V (not 1.8V) - if so, which power rail should be…