Part Number: LMK04806 Other Parts Discussed in Thread: LMK04616 , LMK04832 Hello,
I would like to use the LMK0480x in single PLL mode, see below Fig. 17 from data sheet. Is the OSCin the only possible reference input, or an other input like CLKin1 would…
Part Number: LMK04616 Other Parts Discussed in Thread: LMK04832
I would like to use the LMK04616 in a multi-chassis system, and synchronize them so a SYSREF signal in one chassis is synchronized to a SYSREF signal in a second chassis. My plan would be…
Part Number: LMK04828-EP Other Parts Discussed in Thread: LMK04828 , LMK04610 , , LMK04616 We have a data converter we are using that was designed for use with the LMK04610’s 6-mA HSDS outputs that supplies the inputs for SYSREF and Clock SYNC on the converter…
Part Number: LMK04610 Other Parts Discussed in Thread: LMK04616 Hi,
This is similar to the issue raised earlier. The loop bandwidth for PLL2 is showing to be > 10MHz for a PFD of 10MHz. But this is not observed at higher PFD frequencies.
We need to…
Hi,
We are able to bring up the LMK04610 and LMK04616. But the output frequencies are incorrect. Kindly request you to check the .tcs files attached on the respective EVMs if the required frequency is getting generated.
Regards,
Ayesha
Part Number: LMK04821 Other Parts Discussed in Thread: LMK04616 , LMK04610 , LMK04828 , AFE7686 , CDCM6208 Hello,
We are using LMK04821 in one of the enodeB design.
Currently the reference input of 122.88MHz is applied to CLKIN0.
We have provided option for…
Part Number: LMK04610 Other Parts Discussed in Thread: LMK04616EVM , LMK04616 , LMK04828 , LMK04832 Hi, Team
My customer is using LMK04610, and they would like to keep the output clock has fixed phase delay than input clock.
This can be set by the zero delay…
Part Number: CDCI6214 Other Parts Discussed in Thread: LMK03318 , CDCM6208 , LMK04832 , LMK04616 , LMK05028 , Hi team,
do we have clock translator for below two different condition?
Project 1:
161.132185 CML to 25 LVCMOS
Project2:
156.25 CML to 25 LVCMOS