Part Number: LMK05318BEVM Tool/software: Hello team,
Would it be possible to share the size of this EVM? (Length, Width, Height)
OR is it possible to share the 3D CAD data?
Best Regards, Kei Kuwahara
Part Number: LMK05318BEVM Hi, we are attempting to use the LMK05318BEVM to discipline form a 1pps source. We have use the internal XO and an external signal generator (@12.8MHz) to no avail. With a 1pps signal on PRIREF - we are not seeing the PRIREF_VALSTAT…
Part Number: LMK05318BEVM Other Parts Discussed in Thread: LMK05318B , LMK5B33216 I have a 10 MHz clock signal and I am attempting to create a frequency-syntonized output with a known phase offset.
I have the 10 MHz input connected to PRIREF with the DPLL…
Part Number: LMK05318BEVM Other Parts Discussed in Thread: LMK05318B Hi ,
This is regarding the requirement of configuring the LMK05318B chip for varying reference clock when connected to a Host controller on the final finished product. Since the change…
Part Number: LMK05318BEVM Other Parts Discussed in Thread: LMK05318B I have tryed to following clock generation on the EVB.
Settings and puopose
Input 12.8 MHz from 50ppm SG to XO Input 10 Hz from 50ppm SG to PRIREF Output 8 MHz synchronized to PRIREF edge…
Part Number: LMK5B12204 Hi,
How can the in chip EEPROM be programmed using an external Host controller. Since as of now the TICSPRO Config file is finalised for a specific frequency plan. Hence, the proper sequence of the steps to do the one time EEPROM…
Hi Steven,
Thank you for providing the files. At a glance, I notice that you have SYNC enabled for some of your outputs.
If you program these settings to the EEPROM, after power down, the outputs may or may not be disabled. This is because the global…
Part Number: LMK05318BEVM Other Parts Discussed in Thread: LMK05318B I am trying to use the LMK05318B to lock the 2.5 GHz BAW to an external 10 MHz reference and output 250 MHz. The 10 MHz XO is a high quality Wenzel Oscillator source (so I am not worried…
Update: I have tested the board and saw no issues with the outputs. The previously provided config (attached) outputs 400 MHz as expected given 25 MHz input.
e2e_LMK05318BEVM brand new LMK05318BEVM appears to be dead on arrival_Oct 24 2022.tcs
Regards…
Part Number: LMK05318BEVM Other Parts Discussed in Thread: LMK05318B I have an EVM that I want to load a TICS Pro file from my design. It is working on the design but I am failing a clock phase measurement. I want to measure my exact settings on the evm…