Part Number: LMK05318BEVM Other Parts Discussed in Thread: LMK05318B Hi, team.
I don't have a LMK05318BEVM and I'm going to get one.
I downloaded TICS Pro S&W. Can that support LMK05318BEVM?
I can find not-B version configuration, but I can…
Hello David,
This is a bug with TICS Pro. We have seen this issue previously and have always recommended to just disable the late/missing. Also, you were able to have the 100 MHz be detected with the late/missing enabled when you programmed the device…
Part Number: LMK05318BEVM Other Parts Discussed in Thread: LMK05318B , LMK5B12204 I setup the LMK05318B evaluation board to generate a 140MHz signal using APLL2 on OUT0 and a 100MHz signal using APPL1 on OUT7 with a 10MHz clock on the primary reference input…
Part Number: LMK05318BEVM Other Parts Discussed in Thread: USB2ANY , LMK05318B Hello Team,
Would you be able to help resolve an issue a customer is seeing using the 1-PPS default configuration TICS Pro configuration with the LMK05318BEVM ? The status is…
HI PF,
I tested the .tcs file with a signal generator as an XO input to the LMK05318BEVM. I do not see the LOS_XO_INTR toggle.
When you feed the XO_P to the EVM board, does the EVM use the same supply as your application board? Essentially, the EVM should…
Part Number: LMK05318B-Q1 Other Parts Discussed in Thread: LMK05318BEVM Hi Friend,
In the process of use, it was found that the 4PIN of IC was short circuit after measurement, and the resistance value was about 1ohm. May I ask what causes this situation…
Hi Ryan,
We have just used the LMK05318BEVM card with the file attached, and seeing some very strange behaviour that could be linked with the original issue.
The device is designed to be disciplined from a 1pps source, in the event that the source disappears…
Hi Andrea,
I'm not sure why it got closed, sorry about that!
Could you please share your schematic snippet?
Are you using the LMK05318BEVM (TI eval board)?
Regards,
Jennifer
Part Number: LMK05318B Hi experts:
I am testing LMK05318BEVM. I fed a 15MHz LVCMOS signal to PRIREF input and try to make the DPLL/APLL1/APLL2 to this reference input. However it seems the DLL always failed locking to 15MHz input. I programed the part…