Part Number: LMK05318BEVM Other Parts Discussed in Thread: LMK05318B Hi ,
This is regarding the requirement of configuring the LMK05318B chip for varying reference clock when connected to a Host controller on the final finished product. Since the change…
Part Number: LMK5B12204 Other Parts Discussed in Thread: LMK05318B Hi Team,
We are looking for jitter cleaner device that meet the following specifications.
-System 1 Input =74.25MHz / Output=74.25MHz
-System 2 Input =148.5MHz / Output=148.5MHz
-Hard…
Part Number: LMK5B12204 Dear Team,
My customers have a clock signal with frequencies 80.566MHz, 201.416MHz, 207.5195MHz, 161.1328MHz, 402.832MHz, 415.039MHz.
There is only one clock signal, at different times, possibly at different frequencies as mentioned…
Part Number: LMK5B12204 Hello all,
Assuming VDDO_x is 3.3V, what would be the single ended voltage swing (pk-pk) when driving a 50ohm termination?
Output frequency is 32MHz
I'm measuring about 1.1Vp-p with the above condition, is this what should I expect…
Part Number: LMK5B12204 the question is for your generic BAW based jitter cleaners - are they susceptible to vibrations from fans or mechanical noise like tapping on the circuit board assembly? is there a natural resonance frequency for the mounted BAW…
Part Number: LMK5B12204 Dear sir.
I am thinking about using LMK5B1224 as jitter cleaner.
Is it possible to use LMK5B1224 as jitter cleaner with following condition?
INPUT : 312.5[MHz] with 0.004[UI] period jitter
OUTPUT : 312.5[MHz] with under 0.0004…
Part Number: LMK5B12204 Other Parts Discussed in Thread: LMK05318B
Hello all,
Regarding the above requirement:
For APLL1, APLL2, and Digital Blocks, I should place a nearby 10-μF bypass capacitor on each pin.
I measured the actual voltage on CAP_PLL1…
Part Number: LMK5B12204 Other Parts Discussed in Thread: LMK05318B Hello, I would like you to confirm about below. * I would like to align phase between input clock and output clock by using LMK5B12204. According to datasheet, there is following description…
Part Number: LMK5B12204 Hello,
I like to know the block read operation of this LMK5B12204.
I tried block writing operation and it seems to be done successfully.
But for the block reading, it can only get the first byte data successfully and the other…
Part Number: LMK5B12204 I would like to ask a question how to use LMK5B12204.
Currently, we are using LMK5B12204 and are having an DPLL unlocked issue. In our schematic, PRIREF is tied to FPGA to receive clock signal and to generate audio recovery clock…