Part Number: LMP7731 Hi,
The below graph of the input bias current of LMP7731, I want to make sure I understand what direction these currents have.
Is it per default considered the current direction is into the (+) and (-) terminals?
Thank you
Part Number: LMP7731 Other Parts Discussed in Thread: LMP7721 , OPA392
Hi Team,
I am having trouble finding an op-amp that would satisfy the customer requirements below. The customer finds LMP7731 is close but the data-sheet is lacking key information. …
Part Number: LMP7731 Other Parts Discussed in Thread: TINA-TI , THS4520 , THS4551 , THS4541
Hi Support Team,
Am referring to one of the reference design with instrumentation amplifier. Which is configured as differential mode and with help of TI technical…
Part Number: TPS7A39 Other Parts Discussed in Thread: TPS7A47 , TPS7A94 , TPS7A30 , LMP7731 , TLV2460 Tool/software: Hi, I'm designing a very low noise amplifier circuit.
Do you have something better than TPS7A39? I need to regulate negative and positive…
Part Number: LMP7731 Hi,
What is the recommended shelf life for LMP7731MA/NOPB? Is it okay if we use it with a lot date of Jan 2013 on a noise sensitive board without causing reliability and functionality issues?
Thanks,
Saeedeh
Part Number: LMP7721 Other Parts Discussed in Thread: TINA-TI , LMP7731 , LMC6001 , OPA316
Tool/software: TINA-TI or Spice Models
Dear community,
I'm currently simulating a design with the LMP7731 amplifier and I got simulation issues in OrCAD PSpice (I…
Part Number: LMP7731
Where I can get the value of input capacitance for this OpAmp? I want compare it with ADA4528-1 and this characteristic is important in an application.
Hello Roberto,
The LMP7731 is a low-voltage op amp with an absolute maximum supply voltage rating of 6 V, and maximum input differential voltage of +/-2 V. Beyond those specified maximums no other limits are listed in the datasheet. Very likely the LMP7731…
Other Parts Discussed in Thread: LMP7731 , OPA376 Hello,
Using the LMP7731 with high gain (200), input resistor of 1k and feeback resistor 220k (with parallel capacitor of 4,7nF) to measure low amplitude 50Hz signal, we have very low oscillation problem…
Other Parts Discussed in Thread: LMP7731 , LMP7732 Hello,
The LMP7731, LMP7732 data sheets show the input bias current off the graph as the CM approaches the rails.
With a 5V supply:
1 - Is it safe to run the CM to the rails over temperature?
2 - What…