Hello Andrea,
I took some measurements in the lab and I do think that you may be able to use the A1 output. However, you will need to have a very large impedance between A1 and ground in order to use this as an output. This is because of the internal…
Part Number: LMP8601 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models I am unable to load the P Spice model for LMP8601 into TI-TINA. The file on the LMP8601 page is a .MOD file, but when I try to use that file to create…
Part Number: LMP8601-Q1 Other Parts Discussed in Thread: LMP8601 , INA240 Dear All
I need to sense current in a high side switched inductive load. To protect IC +IN and -IN inputs from going negative at switch off beyond the specified voltage can I clamp…
Part Number: LMP8601 Other Parts Discussed in Thread: LMP8603
Hi Colleagues,
Hope all is well over there, where sun always shines :-)
I have a customer evaluating the LMP8603 and was wondering if we have data to plot the common mode voltage versus supply…
Part Number: LMP8601 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models
Thank you for your patronage.
In the sample circuit below, why does the out voltage start from 2V? I think that it starts from 0 V because nothing…
Other Parts Discussed in Thread: LMP8601 Hello,
I would need further information about the offset output voltage of the LMP8601.
In the datasheet it is briefly mentioned, that a power supply with an internal resistance lower than 10 Ohm should be used…
Other Parts Discussed in Thread: LMP8601-Q1 , LMP8601 , RCV420
Hi,
I'm looking at datasheet for LMP8601, LMP8601-Q1, document SNOSAR2F –SEPTEMBER 2008–REVISED JANUARY 2014
On page 23, it shows an application of using LMP8601 as a 4-20mA Current…
Part Number: ISO124 Other Parts Discussed in Thread: LMP8601 Hello ,
I am planning to use ISO124 to provide isolation as a second stage after my current measurement circuit featuring LMP8601. I might add a second ISO124 for a different reason on the same…
Other Parts Discussed in Thread: INA381 , INA193 , INA200 , LMP8601 , INA282 , INA206 , TMCS1100
Hi,
I design Pulse generation circuit using Op-amp.
Without current sensing amp(INA381), the output signal is no problem.
But, add current sensing amp(INA381),…