Part Number: LMV331 Other Parts Discussed in Thread: LM339 Tool/software: Hello,
Could you clarify, if valid output is guaranteed over temperature for below input and VCC conditions of LMV331.
Device: LMV331I
Vcc+ to GND: 3.2V
IN+ input 4.2V (series…
Part Number: LMV331 Tool/software: LMV331IDCKR IN- impedance abnormal,about 100R to GND.
Our Circuit as below:
IN- also connect Test MCU output IO(0~3.3V).
Which situation can damage IN- to low impedance?
Thanks!
Part Number: LMV331 Other Parts Discussed in Thread: TL331LV , TLV9020 Tool/software: Hi team,
When only use pull up 3.3v logic voltage on output pin(4pin), but don't supply Vcc, we found LMV331 Vcc pin(5 pin) will get unexpected voltage about 1.7V.…
Part Number: LMV331 Other Parts Discussed in Thread: TLV9020 , ALL HI.
As shown in the following picture. The chip specification is the description of the input common mode voltage, the maximum input common mode voltage can not exceed vc-0.7v, beyond this…
Part Number: LMV331 Hi Support Team.
In the Qualification Summary, the results of CDM are described as "See data sheet". However, the datasheet does not show the results of CDM.
Please tell me CDM data of LMV331M7XNOPB.
Thanks,
Yutaro Haya…
Part Number: LMV331 Hi Support Team.
In the Qualification Summary, the results of CDM are described as "See data sheet". However, the datasheet does not show the results of CDM.
Please tell me CDM data of LMV331M7/NOPB.
Thanks,
Yutaro
Part Number: LMV331 Other Parts Discussed in Thread: LMV7275 , TLV1701 Hello,
I have question to ask about LMV331 The circuit design is as follows
When V+ > V-, Vo = VCC When V+ < V-, Vo = GND
But an abnormal phenomenon occurs, when V+ < V-, Vo =…
Part Number: LMV331 Hello Everybody;
The Output of the LMV331 is connected to a capacitor (app 1.5µF @2V): If the LMV331 gets low, the capacitor will be discharged over the output pin of the LMV331. There is no additional resistor.
(The charging…
Part Number: LMV331 Hi all,
In fact, based on the LMV331 datasheet supply voltage range shown below:
Normally, if the Voltage supply is below 2.7V, the output voltage VF2 should be 9V.
Based on the simulation, the output voltage is 0.388V.
I want…
Part Number: LMV331 Other Parts Discussed in Thread: TLV9032 , TLV7011 , TLV7021 Hi team,
what will happen to the output when the power on VCC is not yet 2.5V ?
is there any reset circuit inside that can prevent this unstable phase?
Regards,
Fred