Other Parts Discussed in Thread: LMV761 , LM339 , LMV331-N Hello TI,
If someone can answer whether for LMV761 if an input is close to the VICRmin (-0.3V) and the other is 0V what happens with the bias currents? Are they still in the pA range or do they…
Other Parts Discussed in Thread: LMV339 , LMV331 , LMV339-N Hello TI Support. We are using the LMV339 oparating at 3.3V.
Q1. We need to know, if the output has a known state when the input terminals is at VCC?
Q2. If IN+ is at 2.5V and IN- is liftet…
Hi,Betty,
I uploaded my schematic .
3.No resistor connected between GHX,GLX and CSD88599Q5DC.
4.These resistors are used for BKIN detection.
thank you so much.
Schematic Prints.pdf
Hello Kai and Daniel, Thank you for continuing focus on this issue. Based on your suggestion, I measure the amplifier before Riso and power pin of LMV324. Please refer the attached file. The C461 is 1uF.
The test result is as follows, RISO=0ohm, Vc…
It is in the 19th page of this pdf under the title "2.2.3 Isolated Voltage Measurement Using AMC1200"
I plan to use the charger for the High side power.
tiduby7a.pdf