Part Number: LMX2571EVM Other Parts Discussed in Thread: USB2ANY Using TICS Pro w/ LMX2571EVM. Running on Windows inside a VirtualBox VM, which means I have to manually attach USB devices to the VM after plugging them in.
TICS Pro says my USB2ANY firmware…
Part Number: LMX2571EVM Other Parts Discussed in Thread: USB2ANY , , LMX2571 Hi
Our company create special synthesizer contains two LMX2571, to prototype we use two LMX2571EVM boards and two USB2ANY interfaces to control the boards separately according…
Hi DL, Codeloader is no longer supported. TICSpro is the currently supported GUI to control/communicate with our clocking EVMs. https://www.ti.com/tool/TICSPRO-SW
Here is the LMX2571EVM user's guide - this is a quick start guide on getting up and running…
Part Number: LMX2571EVM Other Parts Discussed in Thread: USB2ANY , CODELOADER , LMX2581 , LMX2571 One of my customers is having an issue where it won't accept the default registers or the ones in Figure 3 of the user guide. It seems to be outputting a random…
Part Number: LMX2571EVM Other Parts Discussed in Thread: LMX2571 , USB2ANY Hello! I am using a micro-controller to interface with an LMX2571EVM. My code for LMX2571 register access seem to be working just fine. When I try to start up (initialize) the…
Part Number: LMX2571EVM In SNAU176A it is said:
On the Ground Layer, Figure 10, notice that there is a separate ground plane below the OSCin signal. This is to prevent the OSCin signal coupling to the other ground plane. They are connected by a resisto…
Part Number: LMX2571EVM Other Parts Discussed in Thread: LMX2571 Hi,
I've been working on the evaluation board for LMX2571.
It seems that the dither feature is not working in the PCB.
The phase noise profile and the spur levels remain the same, even…
Part Number: LMX2571EVM Other Parts Discussed in Thread: CODELOADER , USB2ANY , LMX2571
Good Morning,
I have some problem with set freqencu on LMX2571, we use evo board, usb2any and applications Code Loader 4 to write and read value on register. When we…
Part Number: LMX2571EVM Other Parts Discussed in Thread: LMX2571 , CODELOADER Hello,
I want to generate two cycles frequency with LMX2571 EVM, 235MHz and 280MHz. Register values are configured by default, then alternant switch register R0 to achieve frequency…