Part Number: LMX2572EVM Other Parts Discussed in Thread: LMX2572 , USB2ANY Hello,
I am currently trying to make an automation programming the LMX2572EVM boards through python script.
I got the DLL files from here : SDK link
So far I can do these with the…
Part Number: LMX2572EVM Hi team,
I observed signals on the spectrometer other than those I wanted to observe, why is there clutter and how to remove it?
Thanks
Best regards
Jiahui
Part Number: LMX2572EVM I am working with the LMX2572EVM. I'm presently trying to ramp up 36MHz in 144usec (RAMP0), then ramp back down 36MHz in 144usec (RAMP1), then repeat the process (triangle wave)(using automatic ramping).
Is it possible to do…
Part Number: LMX2572EVM Other Parts Discussed in Thread: LMX2572 , LMX2582 Hi Team,
Good day! I'm posting this in behalf of the customer.
My project involves using the LMX2572 as the synthesizer for a UWB radar system. I was initially going to use the…
Part Number: LMX2572EVM Other Parts Discussed in Thread: LMX2572 , USB2ANY Hi, I need to control the LMX2572EVM via a linux machine. The TICS pro is only available on windows. I have also seen LMX2572_PLL.py which appears to be importing windows related…
Part Number: LMX2572EVM Other Parts Discussed in Thread: LMX2572 Hi sir,
I am using LMX2572EVM Evaluation board I want 122.88MHz frequency at RF out AP port can u tell me which configuration I am set in TICS pro software.
in EVM datasheet it is mentioned…
Part Number: LMX2572EVM The data line resistance values for R5, R8, R9, R16, R19, R20, R22 are all 12Kohm, which I'm trying to understand. With the input capacitance of the digital input pins, I would think this would limit the max bus speed.
The…
Part Number: LMX2572EVM Other Parts Discussed in Thread: LMX2572 Hello,
When testing the LMX2572EVM, the integer boundary spurts vary greatly at different frequencies. The table below show the spurious suppression of deviation is 1M at fPD=100Mhz.
When…
Part Number: LMX2572EVM Other Parts Discussed in Thread: USB2ANY I have purchased the LMX2572EVM and evaluated it, but when I run it with TCS Pro in Default Configuration, it should lock in the 3GHz band, but it oscillates without locking in the 2.7GHz…
Part Number: LMX2572EVM Other Parts Discussed in Thread: LMX2572 , LMX2594 Hi,
I am planning to utilize LMX2572 PLL chip in my design and now I am going to order LMX2572EVM to investigate its performance first.
Question:
I will drive LMX2572EVM with 250 MHz…