Part Number: LMX2572LP Hi,
Our customer is using the LMX2572LP's FSK I2S mode for FM modulation, but only when using VCO core 4 are the spurs getting louder around the carrier. The desired modulation frequency &Diviation is set with the settings below…
Part Number: LMX2572LP With the LMX2572LP, is there any way to put the pin into the MUXout pin 20 into a High Impedance state?
The MUXout pin can be set between lock detect and register readback. In register readback, it behaves like SPI SDO. In order…
Part Number: LMX2572LP Hello,
To replace IDT 5V9885 by LMX2572LP, we are running some case of simulations on TICS pro.
Target EE is video system, it is required 74.25MHz and 74.25/1.001=74.175824175824200MHz output to cover TV monitor filed clock and…
Part Number: AFE7071 Other Parts Discussed in Thread: LMX2572LP , AFE7070 , LMX2572 In some of your app notes, TI recommends using the LMX2572LP to generate the LO input to the AFE7070/AFE7071. The output from the LMX2572LP is more or less a square wave…
Part Number: LMX2572LP Other Parts Discussed in Thread: LMX2572EVM Hello,
I plan to use LMX2572LP at VHF (vide avionic band 118-156MHz), in integer mode, with phase detector frequency 267kHz and 1-st IF 45MHz, then highest 1-st LO frequency multiplied…
Part Number: LMX2572LP Hello,
I plan to use LMX2572LP at UHF, in integer mode, with phase detector frequency in order of 100kHz - of course rectangle shaped. In datasheet, the lower limit for phase detector frequency is however 0.25MHz. What is the reason…
Dear Noel,
We replaced the LMX2572LP with the new one and we used suggested capacitor values. Also, we changed LD_TYPE to 0x0. Unfortunately, problem continues. Additionally, we made a new observation about this problem:
As you know we programming the…
Part Number: LMX2572LP Other Parts Discussed in Thread: LMX2594 , I would like to configure the RFout to be transmitting for short intervals of time, ideally configured by an external input (e.g. SYNC pin?) or configured via register settings.
The sequence…
Part Number: LMX2572LP 購入したLMX2572LP評価ボードについての質問です. LMX2572LPEVM UserGuide SNA235に記載されている10ページ 3.2.4のFSK Modularionについて、FSK変調測定用のTICSPROの設定ファイルを教えてください。 購入した評価ボードのReference PRO基板は、LMK61PDOA2となっております。
I have a question about the LMX2572LP evaluation board…
Part Number: LMX2572LP Hi
I download the Ultra Librarian based data file to generate Cadence OrCAD 16.6 footprint. but it looks the file doesn't work properly. wihle double click the 2020-06-24_08-20-39.bat file, the Allegro can be called , but it…