Part Number: LMX2572LPEVM Other Parts Discussed in Thread: LMX2572LP , TICSPRO-SW , USB2ANY , LMX2571 We want to use an LMX2572LP EVM board to demonstrate that we can set up a deterministic phase relationship between REF input and RF output. But it's not…
Part Number: LMX2572LPEVM Other Parts Discussed in Thread: LMX2572 HI TI expert
I use snau235 LMX2572LPEVM Evaluation Instructions as a reference to design my RF clock distribution system. I found there ware lots of 0ohm resistors placed on the power rails…
Part Number: LMX2572LP Hello,
after attempting to use the phase *** function to phase modulate a signal, it seems this won't work because I can't get the phase to retard as I want it to - it only advances. I am now thinking that the best option to get…
Hi Conor, LMX2572LP would be an equivalent part given the competitor part has an integrated VCO, the part you're considering, LMX2430 is just a PLL .
Regards,
Vicente
Part Number: LMX2572LP Hello,
I'm starting on a design that needs a PLL and some form of phase modulation. On the initial scan of datasheets, the LMX2572LP looks like it might be the best option if it can do both of these together. I realise the device…
Part Number: LMX2572LP Other Parts Discussed in Thread: LMX2594 , LMX2572 Hello,
I'm trying to experiment with the phase shifting functions of the LMX2572LP using the dev board and TICSPRO software. I have it set up to output 400MHz from the standard 100MHz…
Part Number: LMX2572LPEVM Other Parts Discussed in Thread: LMX2594 , LMX2594EVM , LMX2572LP Hi,
Are the design files or step model of LMX2572LPEVM available for download anywhere?
Part Number: LMX2572LP Hello,
is there any data on input impedance on the reference oscillator input and output impedance on the RF outputs?
The datasheet (section 7.3.1) simply says the input is high impedance but I see no value given - can I stick the…
Part Number: LMX2572LP Hi TI Experts,
we are using LMX2572LP in our Digital Mobile Radio at 136-174 MHz frequencies.
We are struggling to solve the spur issues of LMX2572LP at 192 kHz modulating sampling rate.
However, we observed that the spur level…
Part Number: LMX2572LP Hi, I have a question about the ramp frequency range of LMX2572LP. In the datasheet, it reads, this device can generate one frequency from 12.5 MHz to 2 GHz. But what is the ramp frequency range of this device? Because normally …