Part Number: LMX2594 Tool/software: In my application I need to generate a 12.5GHz tone but I need a higher output power. According to the datasheet this device can go higher in power. Does anyone know what to do or check to solve this issue? Thanks. …
Part Number: LMX2594 Tool/software: Hello,
I noticed that your company's LMX2594 chip has frequency scanning capability and I have some questions that need to be consulted. Firstly, how fast can the scanning speed of LMX2594 be? We hope to achieve the…
Part Number: LMX2594 Tool/software: The figure is from LMX2594 datasheet(P28,Figure 27).With about SYNC in category1,when CHDIV = 2,4,6,is it correct that I don't need SYNC signal but SYSREFREQ is necessary?
Waiting for your answer.
Part Number: LMX2594 Other Parts Discussed in Thread: LMK00301 Hello,
We are planning to connect the LMX2594 RF output to the TI buffer (LMK00301) input, which needs a differential common mode voltage of 0.25V to 2.1V (1.2V for our case).
One of our…
Hi Amir,
Phase shifting of our synthesizers use MASH.
We do have some clock devices, e.g. LMK04832, that can support 21ps resolution but the max. output frequency is 3.2GHz.
Hi Abhijith,
If you do not have phase noise requirement, you have to take the trial-and-error approach.
Go ahead and order some MEMS oscillator samples. At the same time, order some crystal-based oscillators having the same package. I also suggest you…
Part Number: LMX2594 Other Parts Discussed in Thread: LMX2595 Tool/software: Hi,
I have a broadband project between two LMX2594 or LMX2595 chips where I want to have deterministic phase across as much of the spectrum as possible from 10MHz to 15GHz. …
Part Number: LMX2594 Other Parts Discussed in Thread: LMX2592 , Hi....,
I just want to know how much overall current it will consume when OUTB is also enabled by the internal register setting?
If any current consumption split up is there like LMX2592 table…
Part Number: LMX2594 Tool/software:
Hello, I am writing with an additional question about the LMX2594. Currently, I need to output frequencies from 13.9GHz to 14.7GHz in 1kHz increments. However, when I start at 13.9GHz and change to 13900.001, 13900…
Part Number: LMX2594 Tool/software: Hi TI,
I have designed a custom PCB using the LMX2594 that operates with both an EXT Clock (Sine wave) and an INT Clock (TCXO: CMOS).
(Attached is the circuit diagram.)
The EXT Clock is input into the PLL through…