Part Number: LP38512-ADJ
Dear E2E,
Please help to cehck whether we have p2p LDO solution with AP7362 SO-8 package?
i found the similar one is LP38512-ADJ, but two portion different, 1) pin define is total oppsite rotation, such as pin 1 in LP part is…
Other Parts Discussed in Thread: LP38512-ADJ Hello,
The So-PowerPAD has a θjc rating of 11℃/W for LP38512-ADJ.
And the TO-263 has a θjc rating of 2℃/W for LP38512-ADJ.
Could you tell me where is the temperature measurement point of this θjc…
Hi Josef,
Unfortunately we do not have anything P2P in fixed-output. The two best options here are TPS7A7001 or LP38512-ADJ. I would lead with LP38512-ADJ as it is the closest match in terms of pinout - LP38512MR-ADJ/NOPB or LP38512MRX-ADJ/NOPB.
regards…
Other Parts Discussed in Thread: LP38512 Hello,
One of my customer have reported LP38512 device failure, when output is shorted to ground to test the short circuit protection of the device. What are the precautions that needs to be taken to avoid this…
Part Number: LMP8646 Other Parts Discussed in Thread: LMZ12003 , LP38512 , Hi,
I am using LPM8646 in my application which similar to Application #2 given in datasheet except LMZ12003, I am using LP38512 - adj instead of it. I want to ask why resistor divider…
Part Number: LP38502-ADJ Other Parts Discussed in Thread: LP38512
Hi team,
My customer is evaluating the device LP38502 now with CR 1A load( input 5v, output 1.2v, use EVM modify it), the start up waveforms are below. The waveform is weird, the output…
To put this into perspective, '4 - 5mV' out of 1.5V represents approx. 0.26% to 0.33% accuracy, vs the LP38512-ADJ native accuracy of 1% to 2%.
While you could probably trim the LP38512-ADJ Vout to this degree of precision under a single specific…