You can use the good old BSL for MSP430F1610. Only 4 signals plus signal ground and power.
P1.1 for serial transmit. P2.2 for serial receive. RST/NMI and TCLK form PC to start BSL.
See: http://processors.wiki.ti.com/index.php/BSL_%28MSP430%29
But do…
David Conde said: a buffer of 512 bytes is created before the main
In other words, it's a global (or, at least, file-scope) - so it won't be on the stack.
The MSP430F2274 has only 1K of RAM in total - so your 512-byte buffer consumes half of that…
Other Parts Discussed in Thread: MSP430F1610 Hi,
I'm compiling assembly code on Code Composer Studio with MSP430F1610 as the target...
The first line of code is
>> .equ DCOCTL, 0x0056
and it generates the error
>> error: expected a decl…
Other Parts Discussed in Thread: MSP-TS430PM64 , MSP430F1610 Hi,
I'm using the code example FET140_FLL_01.C on the MSP-TS430PM64 test board. The processor is MSP430F1610. While debugging, the program goes into an infinite loop on the line of code in bold…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…