Other Parts Discussed in Thread: MSP430F423 , MSP430F423A We use several MSP430F423 on one of our product.
We don’t have any more of them in stock and the suppliers seem to have MSF430F423A in stock.
On TI web site, i see this : SAME FUNCTIONALITY…
Part Number: MSP430F425 Other Parts Discussed in Thread: MSP430F423 , MSP430F6736A , MSP430I2041
Tool/software: Code Composer Studio
I want to implement single phase Energy Meter based on MSP430F423/425/427 Micro controller. Is there any app note for implementation…
Part Number: MSP430I2030 Other Parts Discussed in Thread: MSP430F423 , MSP430F6779A I'm using the ADC24 from MSP430i2030. How could I get the offset values from the ADCs?
I will replace the MSP430F423 µC. At this µC you could short the ADC Inputs to…
Hello James,
thank you, but I would like to know, how I can measure the offset value of the ADC24.
The MSP430F423 has the opportunity to short circuit the ADC input pins internally. After this I can measure the offset voltage.
The i2030 dosen't have this…
Other Parts Discussed in Thread: MSP430FE4272 , MSP430F423 , MSP430F1481 , MSP430FE423
Hello.
1 phase. voltage, current and Power.
-The voltage range is 220v AC.
-The current range is 0 to 20A.
1. Use MSP430FE42x MCU with shunt resistor.
http…
I think you are using MSP430F423, F423A, F425, F425A, F427, or F427A. You have a PCB that copied some of the “features” of the MSP-TS430PM64. It includes a jumper, an LED, and a resistor from pin 12 to ground. Am I correct? MSP-TS430PM64 is…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…