Part Number: MSP430F4784 Other Parts Discussed in Thread: MSP430F6779A , ADS1248 Can someone tell me if the 16-bit sigma-delta ADC block on the MSP430F4784 has a notch filter for 50/60Hz rejection?
Thanks in advance.
Part Number: PCA9539 Other Parts Discussed in Thread: MSP430F4784 , Hi,
I'm currently using PCA9539 I/O expander. interfacing with MSP430F4784, using I2C.
when the IC power up (3.3), does INT pin initially low ? even though pull up is connected (10k…
Part Number: PCA9539 Other Parts Discussed in Thread: MSP430F4784 , Hi,
I'm trying use additional GPIOs for my board ( MSP430F4784), So I'm using PCA9539 I/O expander 16 bit.
As per the datasheet I programmed using I2C.
I'm using 0x74 as slave address…
Other Parts Discussed in Thread: MSP430F427A , MSP430F4784 I want to interface 5V LCD to MSP430F427A / MSP430F4784.
Both processors have Vio = 3.3V. How to interface the processors to 5V LCD?
How to change contrast voltage?
Other Parts Discussed in Thread: MSP430F4784 , MSP430P325 Hello All,
I am using MSP430F4784 in my application.
I want to know the formula for calculating output digital code of SD16_A ADC in MSP430F4784.
It is not mentioned in MSP4304x family user guide…
Hello!
I have some problems with leading out information on the SBLCDA4 in dynamic mode. LCD blinks permanently with some frequency. I connected LCD in appliance with examples of TI and used firmware from official site of TI. Have You ever seen this problem…
Other Parts Discussed in Thread: MSP430F4784 Hello,
I am developing application on MSP430F4784. It has a 16x16 hardware multiplier.
Development IDE is Code Composer Studiio v 5.4.
I want to perform following multiplication:
unsigned int temp1;
unsogned…
Other Parts Discussed in Thread: MSP430F4250 , MSP430F4784 Checked the description of the SD16_A modules in both of the controllers:
http://www.ti.com/lit/ds/symlink/msp430f4250.pdf
SD16_A, input range: Vi - Absolute input voltage range: AVSS-0.1V AVCC
…
Other Parts Discussed in Thread: MSP430F4784 I am using a MSP430F4784 making a/d samples on each of the 4 channels. I have the inputs connected to a bench precision voltage source. I am receiving very stable A to D data with a consistent reading. Leaving…
Other Parts Discussed in Thread: MSP430F4784 Hi all
I have a problem with USCIAB0RX_VECTOR to receive NACK's (I2C)
This code compiles well:
#pragma vector = USCIAB0TX_VECTOR __interrupt void USCIAB0TX_ISR(void) { ... }
This one doesn't:
#pragma…