Other Parts Discussed in Thread: MSP430F5635 Hi ,
I am able to map Port 2 to UCB0 signals .
Is there any way to map Port 5 pins 2 , 3 , 4 to UCB0 - SIMO , SOMI , CLK signals ?
My hardware is designed to get UCB0 - SIMO , SOMI , CLK signals from Port 5…
Other Parts Discussed in Thread: MSP430F5635 Hi
I am new to micro controller programming .
I want to measure the battery voltage that ranges from 8 V olts to 14 volts .
I believe the the maximum voltage that can be measured using ADC12 of MSP430F5635…
Hi,
I have 2 analog signals , one is the battery voltage(signal 1) and other is a device specific signal (signal 2).
They are fed into P6.4 / A4 and P6.5 / A5 of the microcontroller .
The conversion of both the signals will be initiated by the user…
Other Parts Discussed in Thread: MSP430F5635 Hi,
I am using MSP430F5635 .
1. When the user does not use the system ie. when there is no keypad activity , I have to take the controller to sleep mode .
How is this done ?
2. Similarly when the user presses…
Perhaps you're looking for " python-msp430-tools "? Please keep in mind that it's not an official TI tool. See similar threads below.
Error while installing msp430-tools to python on windows 7
Linux/MSP430F5635: Python Firmware Upgrader…
Other Parts Discussed in Thread: MSP430F5635 Hi,
I am working on the project, in which, four MSP430F5635 boards are connected with PC through USB HUB. In software, CDC USB communication class will be used for all MSP430F5635.
By taking reference from…
Other Parts Discussed in Thread: MSP430F5635 Hi,
I have MSP430F5635 which has USB. What all options are available to update the software on this device?
Do I only have USB option avaiable or can I use UART to update software? I read slau319 and it looks like…
Other Parts Discussed in Thread: MSP-FET , MSP430F5635 Working with an MSP430F5635, IAR, TI MSP-FET in JTAG mode.
Nowhere in my code do I enable NMIIE in the SFRIE1 register, but every so often (I suspect due to noise) I end up in my user_nmi_isr trap.…
Hi Todd,
I am currently using the MSP430F5529 which is on the experimenter board, and the code will be ported to a MSP430F5635 after it is confirmed to be working.
If I am not mistaken, only Port 4 of the 5529 has a PMAP register for configuration,…