Hello
I want to generate an internal clock DCO = MCLK = SMCLK of 4 or 8MHz, without any external crystal. is this possible?
How can I set this up?
With an external 32.768kHz oscillator it works like this:
void initClock(void) { // DCO = 32768 * 1 * (30…
Other Parts Discussed in Thread: MSP430FG479 Hi, I have been using this msp430fg479 chip for quite some time. Used to use only 1 channel of the available ADC channels, but now I need to use 3 channels concurrently. and I'm having problems getting the readouts…
Part Number: MSP430F6736 Other Parts Discussed in Thread: MSP430FG479 , MSP-TS430PZ100 , , MSP-FET Hi - trying to find out why I am not able to get MSP-FET430UIF to work with my version of IAR.
I used this interface (IAR/debugging tool) before to debug with…
Hi Prithvi,
the same ADC (SD16_A) is also in MSP430F(G)47x (see Table 2-1 in www.ti.com/.../slaa957.pdf ), which have INL specified in the datasheet.
www.ti.com/.../msp430f478.pdf (see 5.26, page 31) www.ti.com/.../msp430fg479.pdf (see 5.26, page 31…
Dear
Thank you for your suggestion.
I have ordered MSP430FG479 sample just before. About the option 2, I need several analog inputs
for my application. So it is better that I can use analog inputs more than 2 (not only A3 and A4) with
1 DAC available…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…