Part Number: MSP430FR2110 Hello everyone, Use MSP430FR2110. MCLK is 16MHz. The required specification requires a startup time of 40 ms or less. I would like some data on the convergence characteristics of FLL lock.
Thank you in advance.
Best regards,
k.…
Other Parts Discussed in Thread: MSP430FR2110 , ESD351 , ESD321 , ESDS314 , ESDS304 Hi,
I am trying to select an appropriate ESD to protect a MSP430FR2110 GPIO input pin (P1.3). I need to rate the end equipment according to UL639 requirements of 10kV.
Requirement…
Hi K.saito,
I contacted you on E2E by private message to further discuss this issue. I close this post and we can discussed this issue via email.
Best Regards
Johnson
Part Number: MSP430FR2110 I am using MSP430FR2110 and trying to setup a pin interrupt on P1.6. The code is avaiable below. I am having an issue where pin interrupt is not generated when voltage level transition from high to low on pin P1.6. I happen to…
Part Number: MSP430FR2110
I am using the MSP430FR2110. I want MSP430FR2110 to exit LPM3/LPM0 when RTC interrupt is triggered and enter LPM3/LPM0 otherwise. However, RTC clock interrupt stops after short period of time. am I not using the enter and exit…
Part Number: MSP430FR2110 Hi Forum,
This part has 8 P1 and 4 P2 I/O pins. At the top of the datasheet it says 4 P1 pins and 4 P2 pins have interrupt status.
In the fine print under the I/O section of the datasheet, it says that these pins have "edge interrupt…
Part Number: MSP430FR2110 Tool/software: Code Composer Studio Dear team,
I am using MSP430FR2110 and i want it in LPM3 WITHOUT External 32.768kHz.
I tested it without External 32.768kHz and the current was 17uA ( i want less than 3uA). It is too high. …
Part Number: MSP430FR2110 Other Parts Discussed in Thread: MSP430FR2000 , MSP-FLASHER , MSP-FET Tool/software: Code Composer Studio I am using:
the MSP430FR2110
the MSP_FET Flash emulation tool
Code composer
Mac computer
After running the code to put…
Part Number: MSP430FR2110 Tool/software: Code Composer Studio HI Forum,
Happy Holidays to all !!
This is one of those parts in the design where no matter which way you turn, it never works.
The part number now is MSP430FR2110. There are only 8 interrupt…