Other Parts Discussed in Thread: MSP430FR6979 Hi,
I am using the following code to read the internal temps and I get erratic readings, 83, 79, 80, 78, 92, 79...
What would cause this, and how to mitigate?
Thanks, Tom
while(REFCTL0 & REFGENBUSY…
There are signs that the following members are coming. Any hint when?
MSP430FR4131, MSP430FR4132, MSP430FR4133 MSP430FR5887, MSP430FR58871, MSP430FR5888, MSP430FR58881, MSP430FR5889, MSP430FR58891 MSP430FR5986, MSP430FR5987, MSP430FR59871, MSP430FR5988…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
V6MSP430.dll.txt V7MSP430.dll.txt Hello Jace,
The first file is V6 DLL and second file is V7 DLL. I had to add the .txt extension since uploader won't allow .dll
Dave
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…