You could connect MSP430G2544 BSL-TX and UART-TXD in parallel to DM8127 UART-RXD.
And also, DM8127 UART-TXD to MSP430G2544 BSL-RX and UART-RX in parallel.
Other Parts Discussed in Thread: MSP430G2544 Hello,
Do you know what the longevity for the following devices would be?
MSP430G2544
MSP430F2252IDA
MSP430F2242!RHAR
MSP430F5151IDAR
MSP430F5151RSB
IF they were to be EOL'd would there be a pin for pin replacement…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…