Part Number: MSP432P401R Hi all, the idea of this little program is to be able to read the value of a potentiometer using the ADC of the MSP432P401R. To get a more accurate measurement I calculate 4 values and average them and assign them to the variable…
Part Number: MSP432P401R Hi, the idea of the project is to detect the Back Electromagnetic Force (BEMF) of a BLDC and for this I have made this simple program where I wanted to use the ADC of the MSP432P401R in differential mode, since I have used six…
Part Number: MSP432P401R Hi Support Team ,
Regarding the MSP432P401R and BOOSTXL-CC3120MOD , I would like to know the following questions.
MSP432P401R as External MCU and BOOSTXL-CC3120MOD as NWP
and I measure the current in Always connected mode the…
Part Number: MSP432P401R Hello, my project idea is to rotate a BLDC motor by imposing a certain duty cycle value (which I change with Launchpad buttons) and setting a period value (in this case 1 ms) that allows me to make transitions between 6 states…
Part Number: MSP432P401R Hello, I have made a code that allows me, by pressing the button P1.4, to change the direction of the H-bridge having that, if you had activated the high transistor of phase B and the low transistor of phase C and you suddenly…
After changing the DCO frequency the following error started appearing: CORTEX_M4_0: Error initializing flash programming: Your XMS432P401R material is no longer supported. We recommend you moving to production-quality MSP432P401R/M silicon by ordering…
Hello,
After isolating portions of the code used for transceiver mode, I have found the source of the issue.
There were a couple lines inside my transceiver functions that allowed a successful connection to occur after exiting. They are attached below…
Part Number: MSP432P401R Hi,
I am having trouble getting my CC3100 Boost to operate as a MQTT client in CCS composer. I have an example code running in Energia that works great, but I am developing labs for an IOT course and I need things running in CCS…
Part Number: MSP432P401R Hi, my goal would be to be able to control the duty cycle value externally. For this I have thought of using the two pushbuttons that the MSP432P401R Launchpad has, that is, the S1 (P1.1) and S2 (P1.4). For this I post two codes…
Part Number: MSP432P401R Hi
I am trying to operate the RTC without success. I can read RTCTIM0 and RTCTIM1 register stuck with initial value and the HOLD bit on RTCCTL1 stuck at '1'.
I put a breakpoint just after writing to the HOLD bid and verify…