Part Number: MSP432WARE
Hi all,
I am now creating a project with ADC14 but the AD result seems like a wrong value.
These are the code,
I have set P8SEL0 and P8SEL1 of ADC input channel.
unsigned long AD_Converter(unsigned short channel)
{
unsigned…
Part Number: MSP432WARE Hi Team,
I am trying to load a project in CCS Cloud on MSP432P401R Microcontroller. The device is getting detected in the resource explorer page, but the website is not responding when i click on proceed. I couldnt see the same…
Part Number: MSP432WARE Other Parts Discussed in Thread: UNIFLASH Hello,
I am trying to flash the program using BSL scripter on MSP432 launchpad. I have used BSL software invocation method as mentioned below. It gets stuck on the initialization.
MODE P4xx…
Part Number: MSP432WARE Other Parts Discussed in Thread: SYSCONFIG , I opened the Ftsd routine from the SDK, but I can't comoile the process normally because I can't find the following file, I know this is
sysconfig file, but after I downloaded it…
Part Number: MSP432WARE Customer would like to know which API should used to clear Uart status flag? We check the MSP432 driver lib UART function as below and cannot find the API function to clear uart status.
Part Number: MSP432P401R After some study of MSP432Ware 3.4_xx and experiments with timer_A0 interrupts that don't activate themselfs there must be reason
Example used below is not driverlib, it's a pure register level example using one timer and…
Part Number: MSP432WARE Tool/software: Code Composer Studio In projects that set DEBUG (e.g. through the Predefined Symbols), several ASSERT statements fail in dma.c because they look for the DMA pointer. Instead, it looks like these should test for DMA_Control…
Part Number: MSP432WARE Other Parts Discussed in Thread: ENERGIA Dear Comrades!
If someone could please advise whether such is possible? First of all, I am a pianist, not an engineer, so if I am asking something silly, please bear with me. I have a bit…