Part Number: PGA309 Other Parts Discussed in Thread: MULTI-CAL-SYSTEM , To whom it may concern,
I initially tried to use the supplied RS-232 cable to communicate to the HP34401A VOM with the Multi Cal system. After setting up the multimeter I could not…
Part Number: PGA309 Luis,
In the interest of moving forward I realized the system verifies communication and configures the attached PGA309's before proceeding to the calibration steps. I connected my PGA309 PCB's to the Multi-cal system to verify this…
Part Number: MULTI-CAL-SYSTEM Other Parts Discussed in Thread: PGA309 , PGA309EVM-USB ,
Since there is not a PGA309 Test PCA available for the Multi-Cal-Sytem, is there any way to connect the PGA309 test board from the EVM kit to the multi-cal system so…
Hi Todd,
I found the R5_2 and R5_3 images have the same definition for OCRAM in the linker command file. I updated the R5_3 linker command file (attached below), and it works now. Can you please check if it works for you?
Regards, Frank
linker.cmd
Hi Zhang Liang,
Unfortunately none of the PGA devices using an internal M0 Arm processor have mass production support tools. The closest devices with production support are from the Precision Amplifier group that are purely analog devices (PGA308 and…
Part Number: PGA309 Other Parts Discussed in Thread: MULTI-CAL-SYSTEM Dears,
i used multi cal system P GA3 09 in production line to configration with One-Wire Interface. But some PGA309 with own sensor boards will be configrate failed.
Hardware is ok, if…
Part Number: MULTI-CAL-SYSTEM Other Parts Discussed in Thread: PGA309 I'm having trouble using the MULTI_CAL_PGA309 installer. I get to the following point and then cannot continue past this:
Since this computer already has the NI software installed…
Part Number: MULTI-CAL-SYSTEM Other Parts Discussed in Thread: PGA308 , PGA309 I installed the Multi-Cal-EVM program on a PC with newly installed Windows 10 and brought the existing scripts and settings,
but the error "-410" on the 34401A does not work…
Part Number: PGA309 I have seen a forum post about the Multi-Cal PGA309 software source code where there are links to download. The links have since expired. I wanted to see if anyone could provide the LabVIEW source code for the Multi-Cal PGA309 software…