Part Number: OPA2333-HT Hi,
I would like clarification on the bare die dimensions figure on page 4 of the datasheet. What does the 38 µm extending from the die dimensions? Is this the scribe length?
Also, in table 2 what does A,B,C and D indicate…
Part Number: OPA2333
https://www.ti.com/lit/ug/slau502/slau502.pdf AN web link attached here.
------------------------------------------------------------------------------------------------
Hi expert,
If we only look at the first-stage current sink generator…
Hi David,
The HT op amp up to 200C is scarce. OPA211-HT and OPA2333-HT are the only ones that operating temperature range.
https://www.ti.com/amplifier-circuit/op-amps/precision/products.html#1498=HiRel%20Enhanced%20Product%3BHigh%20Temp&sort=1192;d…
Part Number: OPA2333
1. The following circuit of opa2333 is shown in the figure. Is R7 required? Why?Are other operational amplifiers needed?
2. Can internal clamping diodes be used? In case of over-voltage, the clamping diode current is 0.7ma, less…
Part Number: OPA2333-HT Other Parts Discussed in Thread: OPA2333 , Hello,
I am using the OPA2333 in my application to reduce components to help achieve my design size restraints. I am wanting to use a single OPA2333 device to buffer two separate ADC inputs…
Part Number: OPA2333 Other Parts Discussed in Thread: INA333 , , OPA333 Hi!
I'm Jacob, I have been learning the operation amplifier. Now I need to know the inner structure of OPA2333AIDGKR and some theory about it. If you have any papers, please send…
Part Number: OPA2333-HT 1. Can these dual Op-Amps be connected in parallel to provide a higher current output?
I've read this other e2e discussion on the risks of paralleling op-amps, however, it doesn't state it is impossible.
2. If it can be…
Part Number: OPA2333 Hi team. I'd like to know about the input noise accuracy. The input noise is typ value. Is there Min and Max value as a reference value. If you don't have it, I'd like to know what the Max/Min is likely to be. My customer is…
Part Number: OPA2333 Other Parts Discussed in Thread: OPA333 , BUF634 Hi Team,
My customer designs a scheme to increase capacitive load ability, as shown below. They want to check two things with product line:
1. Is this scheme is workable or not?
2. If…
Hi Ammar,
Since the operating temperature range of -65C to 140C very wide, it is difficult to select a part with radiation harden + high operating range in combined specification.
I think that you may have to go with discrete design approach for the 4-20mA…