Part Number: OPA2333-HT Hi,
I am looking to collect temperature data from a k-type thermocouple. The amplifier has to survive at a high temperature greater than 150C. Can I use OPA2333-HT and what should I do for temperature compensation?
I used MAX31850K…
Part Number: OPA2333A-EP Other Parts Discussed in Thread: OPA2333-Q1 Hi,
The specs say that this part is Qualified for Automotive Applications. Does it mean in passed Passed AEC-Q100 or just AEC-Q200?
Munir
Part Number: OPA2333-HT Other Parts Discussed in Thread: INA129-HT Hi, we have an application that will require sensors for monitoring continuosly 4 years at a temperature of 135 celsius. I look to use OPA2333-HT or INA129-HT for the amplifier (the sensor…
Part Number: OPA2333-Q1 OPA2333AQDRQ1 One of the AMPs is not used. What should I do with the unused pins?
The current processing is:
5pin: pull down ground
6pin, 7pin connected together
Is this okay? Any other suggestions?
Part Number: OPA2333 Other Parts Discussed in Thread: LM7705 , OPA333 The circuit schematic is shown below.Using OPA2333 as a voltage follower. The conversion error is large, why?
FLUKE(754) test circuit at 30 ° C. UA=1V. U B = 0.9983V. UC = 0.9997V. …
Part Number: OPA2317-Q1 Other Parts Discussed in Thread: OPA2333-Q1 , OPA2137 , Hi team,
Our customer is looking for low offset and EMC torelance dual opamp, because they are in trouble with the EMC test of the system.
Although they can evaluate only OPA2333…
Part Number: OPA2333-HT We are running tests on a circuit operating up towards 200 to 210 C and using an OPA2333-HT to source a constant 1 mA current through a platinum RTD. We begin to see the RTD measurement go off-course above 155 Celsius, which our…
Other Parts Discussed in Thread: OPA2388 , OPA2333 , TLV2333 , OPA2333-Q1 , OPA2378 Hi all,
I am looking for a P2P replacement of MCP6V02-E/SN.
Could I have your help here?
Thank you!
Sincerely,
Karen
Part Number: OPA2333-HT We have had an OPA-2333HD (plastic package) fail, possibly due to static damage. We have sent the failed sample, along with some new unused items away for decapsulation and analysis. The unusual pad formation makes acid etching…