Part Number: OPA2348-Q1 Other Parts Discussed in Thread: OPA2348
When the OPA2348 is used as a negative feedback signal amplification circuit, I added the 660pF capacitors at the "+" and " -" input to ground for improving interference…
Part Number: OPA2348-Q1 Is the input offset voltage maximum value indicated in the datasheet in both directions or is it only in the positive direction?
Are the two op-amps in the IC separate of each other in terms of input offset voltage or are they…
Part Number: TPSI2140-Q1 Other Parts Discussed in Thread: OPA2348 , Hey TI Expert,
We are designing an Isolation Measurement Device for HV EV Application.
We are using the OPA2348 opamp to measure the Isolation leakage current after the TPSI1240 stage referring…
Part Number: OPA2348-Q1 Hi team,
Could you please give some guidance about how to calculate the worst-case output error of this amplifier? Besides the accuracy of peripheral resistors, what parameters should be taken into consideration? How to use these…
Part Number: OPA2348-Q1 Hi Team
OPA2348-Q1 mentioned "Refer to Circuit Board Layout Techniques, SLOA089" as below captured.
BTW,,, customer cannot find out SLOA089 on TI website.
may I get the document of SLOA089 ?
Part Number: OPA4322-Q1 Other Parts Discussed in Thread: OPA2348-Q1 , Hello TI Team,
I am using both of the above op amps (OPA4322-Q1 and OPA2348-Q1). When these op-amps are off ( It is possible that (+) input voltage can go up to 16V through a 49.9k resistor…
Part Number: TIDA-01513 Other Parts Discussed in Thread: ISO7741 , ISO7710 , ISO7741-Q1 , ISO7761 , ISOW7841 , ADS1118 , , OPA2348 Hi Team
I would like to use the insulation leak measurement circuit insulated from a 1000V battery.
1. We believe that the circuit…
Part Number: OPA348-Q1 Other Parts Discussed in Thread: OPA4348-Q1 , , OPA2348-Q1 , OPA2348 , OPA4348 , OPA348 , TLV3701 , TLV3702 , TLV3704 Hi Team
my Customer has the following questions about FIT for OPA348-Q1/OPA2348-Q1/OPA4348-Q1.
may I expect your swift…
Hello Vedran,
Your understanding is correct.
This issue can be solved by measuring and calculations systematically. As per TIDA-01513 we have 3 measurements.
1) Pack Voltage
2) ISO POS
3) ISO NEG
We have two switches S1 and S2. Pack voltage might…
Other Parts Discussed in Thread: OPA2348 , OPA4348-Q1 , OPA348 Hi Team
inOPA348-Q1(OPA2348/OPA4348-Q1) datasheet,
there is no comment on the Abs Mas voltage for the differential input voltage.
may i know it ?