Hi Astro,
the phase shift is caused by the finite open loop output impedance of OPAmp. An ideal amplifier would have a zero Ohm output impedance. But real OPAmps differ from that. The OPA365 with its strong output stage and higher supply current provides…
Part Number: OPA365 Other Parts Discussed in Thread: LMV793 , SM73302 , OPA607 , OPA863 Hi team,
May I know if we have p2p replacement for OPA365AIDBVR or OPA365AQDBVRQ1? Customer is using OPA365 Q and non-Q part but facing supply shortage. I'm checking on…
Part Number: OPA365 Other Parts Discussed in Thread: OPA607 Dear support team,
May I have your double check the OPA365 supply voltage maximum is correct or not?
Due to the recommended and maximum ratings are all 5.5V.
As I knew, maximum rating is usually…
Part Number: TMS320F28034
Hello,
I'm designing a BLDC drive unit and I'm using the TMS320F28034PNS as microcontroller. One of the design requirements is to be able to read the temperature of the BLDC motor winding using a thermistor sensor. I need…
Part Number: LM27762 Other Parts Discussed in Thread: OPA365 , INA126 , TPS65133 , LM27761 , LP5910 , TPS7A13 Hello,
I would like to discuss the posssibility of using one LM27762 to supply positive and negative 2.5 V to power up around 10 OPA365 and an instrumentation…
Part Number: OPA365 Other Parts Discussed in Thread: TINA-TI , Hello
I have designed simple 0.7V reference voltage follower buffer circuits with TINA-TI
I choose OPA365 because it have IN/OUT Rail to Rail and high Current supply with High Bandwidth, good…
Part Number: OPA365 Other Parts Discussed in Thread: , LMV793 , OPA607 , LMP7717 , Also, could someone from TI provide me with an update on lead times/stocking levels at TI and distys for OPA365AIDBVT.
Part Number: OPA365 Hello,
My customer has adopted our recommended analog pulse width modulation as the following link:
www.ti.com/.../slau508.pdf
However, they found their circuit is easily interfered by 300MHz~400MHz RF emission, even the circuit has…
Part Number: OPA365 Other Parts Discussed in Thread: LM7705 Hi TI expert
What is the risk (damage or relability only ) when the amp. is biased with +5V connected to V+, and V- is connected to 500 OHM resistor which the other end of the resistor is connected…