If you need an ultra low input bias current, like max 4pA at 125C, LMC6484 is the only quad we may offer. If you may tolerate higher IB, we have several quads in smaller packages: closest LMP7704 in TSSOP package as well as OPA4191, OP4192, OPA4196,…
Hi Rico,
Thank you for your post. I can help you find a quad-channel alternative. Please take a look into our OPA4191 and let me know your thoughts.
-Tamara
Part Number: TLC2274 Other Parts Discussed in Thread: OPA4991 , TL3474 , OPA4191 , OPA4192 , OPA2156 Hi, I usually used TLC2274 for op-amp as buffer circuit.
(Connecting In- to Out. Gain = 1)
I want to use more faster slew rate op-amp with rail to rail. …
Hi Paul,
Take a look at the OPA4191. The 1k cost is a bit higher than the price you list. Cost is something you could discuss with your TI sales rep.
www.ti.com/.../OPA4191
This is a very modern, high precision op amp featuring:
Low Offset Voltage…
Hi Charles,
I know what is going on. You are applying the OPA4188 amplifier section as a comparator, with a 2.21 V reference voltage applied to the inverting input. When you drive the non-inverting input to the 1.45 V level you forward bias one of the…
David,
We have several quad op amps with the input common-mode voltage range beyond both rails; please see take a look at OPA4191, OPA4192, OPA4196 and OPA4197.
Alex, I've just tested the circuit replacing OPA4188 for the OPA4170. It performed as expected, without any distortion. I tested it with input frequencies as high as 40 kHz (4 times higher than the actual input maximum) and didn't get any distortion…
Part Number: OPA4188 Other Parts Discussed in Thread: INA149 , OPA4191 , OPA4192 , TINA-TI Dears,
I want to sampling the BUS voltage, the total voltage is about 800V(DC). I have adjusted to about 50V through precision resistance voltage divider, and then…