Part Number: OPA615 Other Parts Discussed in Thread: OPA860 Hi,
In peak detector with OPA615, it is used BAT17 Schottky diodes at C_Hold pins. Is there any special reason for these diodes?
Part Number: OPA615 Hello,
In below figure is the reference design of a Integrator using OPA615. It mentions that Hold control signal is tie high so that this integrator will be free running. I wonder if the hold control signal is drive low, does it…
Hello Nick,
Hopefully, the video decoder issue is an easy fix. For adjusting the internal DC level shift, this unfortunately will not possible unless an external shift is used. The 150mV voltage shift, gained by 2 is a total of 300mV voltage shift at…
Part Number: OPA615 Other Parts Discussed in Thread: OPA860 , OPA695 , Hello experts,
I am working in a tough design where we are trying to measure the peak value of very fast pulses. The pulses are shaped as a double exponential, with a rise time of around…
Part Number: OPA615 I use the OPA615 to sample and hold positive pulses。
Can OPA615 provide only the positive power? Can the "-VCC" pin be connected to ground?
thanks!
Part Number: OPA615 Other Parts Discussed in Thread: OPA860 Hello Guys,
Our customer is looking to to measure the peak value of an optical-pulse signal (converted to an electrical signal via the DET10A2 photodiode, ThorLabs). The pulse has a rise time…
Part Number: OPA1S2384 Other Parts Discussed in Thread: OPA615 , OPA860 , OPA1S2385 Tool/software: Hi team,
The customers want to select an op-amp and the requirement is as below:
Differential signal to single-ended signal 3.3V supply, input signal differential…