Part Number: PGA308EVM Hi there, I am currently using the PGA308EVM and am trying to test several gain values but am running into a problem where the Set Vin value is not being read properly by the software and USB DAQ. For example, I have Auto Vin Vdif…
Part Number: PGA308 Good day,
I am running into a problem with PGA308 when programming OTP memory. All OTP registers return 0xFF. The system is powered off of 5V power supply the entire time.
Here are my calibration steps:
1) Run calibration loop in Software…
Part Number: PGA308 Hi,
In the User's Guide (Literature Number: SBOU069B) about PGA308, Complete Scaling Example is shown on 3.3.1.
There are Step1 - 13 for the scaling. Do you have any idea about we don't use this step.
For example, skip the…
Part Number: PGA308 Hi,
We think the force sensor and PGA308 connects with a connector (JST GH connector, gold plate) below.
Sensor (stand alone, in/output resistance: 500ohm) --- connector (gold plate) = board connector (PGA308) *Power supply: 3.3V
Do you…
Part Number: XTR116 Other Parts Discussed in Thread: PGA308 Tool/software: I'm using an XTR116 in conjunction with a PGA308 for 4-20mA conditioning on a full bridge sensor. All grounds appear to be tied to I-RET except for the EXC- of the full bridge…
Hi John,
Thanks for the additional background. The PGA308EVM is a designed to evaluate the performance of a typical PGA308 device, or more specifically, the sample PGA308 device that is populated on the EVM. This tool is commonly used during the design…
Part Number: PGA308 Hi,
I have the same problem with ”PGA308: PGA308 EVM in Windows 7 or Windows 10”.
Computer discovery equipment and display “USB\VID_0451&PID_2136\5&21900AB8&0&2”.
Please help me to confirm and…
Part Number: PGA308 Please tell me about the operation when used in software lock mode.
After "Run from RAM", "DIS OUT=1 CFG2 Register[D13] is executed. Is this loop processing performed by an external command? Or is it performing loop processing…
Part Number: PGA308 Other Parts Discussed in Thread: XTR116 Hi,
I'm making a 4-20mA 2-wire calibration device. The PGA308 Vout voltage, how to calculated only knowledge with current. For GDAC and ZDAC values.
Mert
Part Number: PGA308 Other Parts Discussed in Thread: PGA309 Hello,
1- PGA308 How to calculate the capacitor (C14) value between Vsj pin and Vout. I didn't see any examples in the technical documentation.
2- What is the reason for using R10 resistor…