Part Number: PGA5807A Other Parts Discussed in Thread: VCA5807 , PGA5807 I have a design using the VCA5807. I am investigating switching to the PGA5807 as a drop-in replacement primarily for the smaller package size. However, from the datasheet, I do…
Hi,
Yes, you can refer to PGA5807A datasheet page 17,
It shows that: The LNA input can be applied either directly or through an ac-coupling capacitor.
Thanks!
Best regards,
Chen
Part Number: PGA5807A Dear E2E,
Do we have LNA solution which spec is shown in below?
Operating Frequency 734 ~ 960MHz
Gain 13 dB
NF 1.1 dB
Supply voltage 1.5~3.3V 2.8V (typ.)
BR,
Jason
Part Number: PGA5807A Other Parts Discussed in Thread: PGA5807 I'm using pga5807 to amplify 5mhz 500mv, single ended signal, but the output is not big enough,and distortion.
my sch is as follows, whether the input and output is connected directly or…
Part Number: PGA5807A Other Parts Discussed in Thread: PGA5807 Hello everyone,
in the last few hours, I tested the LTspice simulation model of the PGA5807.
If I compare the low-pass filter response of the datasheet to the filter response of the simulation…
Hi Dear Customer,
How are you?
Please look at the PGA5807A user's guide page#47.
For example when you connect your input signal at the J10 SMA connector
" SMA_CH5(PGA_CH1) " and also your input signal freq range is running
between 1kHz to…
Hi Adeniji,
How are you?
Thanks for using PGA5807A device.
The data sheet did not mention resistance spec.
Could you please let us know what frequency of the signal
when you are running PGA5807A?
Thank you again!
Best Regards,
Chen
Hi Rizwan,
Yes you should be able to use either of the differential channels for your evaluation with the ADS52J90 EVM.
For your product, if you are looking for multichannel PGAs, then you may want to look at the PGA5807A.