Part Number: DRV2700EVM Hi experts:
I'm trying to drive my piezo speaker with DRV2700EVM, but Piezo Control Console crashed when I click console, my PC OS is Win7.
if I use analog input by an external signal, just connect JP7,JP8,JP9 to PU, remove jumppers…
Part Number: DRV2700EVM I have tried downloading the Piezo Control Console on a variety of devices and all of them are outputting the same error message when I attempt to connect the board to the computer. I want the board to be able to boost an AC signal…
Hi Sydney,
Thank you very much.
I closed JP13,
I enabled output via the Piezo Console.
And with a multimeter I measured 22V between OUT +/ -.
This gives you a small sign of operation.
However, my Jumpers JP7, JP8, JP9 are
In EN/MSP
GAIN 1/MSP…
Part Number: DRV2700EVM-HV500 I installed the Piezo Control Console (1.2.9) on to my Win 10 machine and it does not run?
Mu goal is to create a custom wave form so I can run my Piezo pump
Thanks
Amin Godil
Part Number: DRV2700EVM Hello TI,
I have just bought a DRV2700EVM and have installed the Piezo Control Console V1.2.9 to control it for evaluation. When I connect to the EVM from the PC, as soon as I select 'Console' the Piezo Controle Console has an…
Hi Soumyajit.
Welcome to E2E!
Q1) It is not possible to use 10MHz signal with DRV2667. the output voltage will roll-off before 20kHz.
Q2) Here is the frequency range that can be achieved based on PVDD (reference DRV2700 Datasheet)
Q3) the USB2ANY is…
Other Parts Discussed in Thread: DRV2700EVM I'm trying to evaluate the DRV2700EVM, and running Piezo Control Console version 1.2.9.0. Piezo Control Console sees the USB EVM, I click the "connect" button, but when I click "console", I get the following…
Hi Gareth,
Yes, the DRV2700EVM-HV500. this is the DRV2700 in a flyback configuration. it is capable of outputting up to 500V peak. the output is single ended and can generate a square wave.
This EVM also has a GUI to control the board. Piezo Control Console…