Part Number: DRV5825PEVM-AMPS097 Other Parts Discussed in Thread: DRV5825P Hi there,
The goal of our project is to build an amplifier for a parametric speaker (ultrasonic transducer array). Wherefore, we need to amplitude-modulate the carrier frequency…
HI Yuto,
As I understand you are using the DRV2700EVM-HV500
If that is the case you can use Piezo Control Console GUI to update the firmware over USB
Help-> Firmware Update, and then follow the on screen instructions
Regards,
Arthur
Part Number: DRV2700EVM-HV500 Other Parts Discussed in Thread: LDC2114EVM , , LDCTOUCHCOMCOILEVM , DRV2700 Hello,
I would like to ask some questions regarding trigger operation. DRV2700EVM-HV500 can be used in trigger mode. What kind of signal is needed…
Part Number: DRV2700EVM Other Parts Discussed in Thread: PIEZO-CONSOLE
Hello,
My customer is trying to connect to the GUI and is having some issues. They have downloaded and installed:
DRV2700EVM Firmware v1.7 (Rev. A) – SLOC324A.ZIP
PIEZO-CONSOLE…
Dear Luis,
All jumper settings are in the default settings on the board.
I am currently using the Launch Piezo Control Console 1.2.9 version of the Piezo Control Console
And, no piezo control console while pressing the button does not recognise the device…
Hi Cherry,
Please see this other thread. https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/515391/drv2700evm-and-piezo-control-console-error
following the above threads advice you should try updating the firmware on the…
Hi Arun
If you have not already I would recommend you read the DRV2700EVM-HV500 Users guide because it will explain how to calculate the HV output in some detail (specifically sections 4.1) slou407a
From your perspective. Since you want to change the DC…
Hi, Akaba-san,
Actually, the DRV2700EVM is already compatible with the Win10 version.
In case you are having troubles with the EVM, I recommend to perform a firmware update in the Piezo Control Console. This E2E thread is an example of how to perform…
Hi, Ian,
In the Piezo Control Console, there's an option in the Help Menu called "Firmware Update". After clicking on this option, you will see a new window called "EVM Firmware Updater". You just need to follow the instructions in the window to update…
Part Number: DRV2700EVM Purchased the DRV2700EVM evaluation module.and have installed the Piezo Control Console V1.2.9 to control it for testing Piezo actuators When I connect to the EVM from the PC, as soon as I select 'Console' the Piezo Controle Console…